Part Number: TUSB2E22 Hi
I have test case where I'm driving eUSB signal data as clock to check my TUSB2E22 circuit
the design is copy from TI reference
the signal is 400mv Pk-Pk differential input to edp0/edn0, I see the signal comes in but no signal…
Part Number: TUSB2E22 Other Parts Discussed in Thread: TS3USB221E , TUSB216 , TUSB1064 Hello TI team
The MacPro typec receptacle USB2.0 can only work A6 A7 or B6 B7 that mean when the device directly insert receptor the A6 A7 PIN work USB 2.0 ,and flipping…
Part Number: TUSB2E22 Hello,
Do we have the supply current information about different work state? For example, under the conditions of internal LDO disable or enable, what is the power supply current? Our customer found that the power consumption is…
Part Number: TUSB2E22
Dear Expert ,
Good day!
1.
Our customer find the datasheet of the TUSB2E22YCGR have 2 different working temp range description: 0-70°/-20-85° , in the Recommended Operating Conditions , Ta is -20-85° , in the PACKAGING…
Part Number: TUSB2E22EVM-CAT Hi
in TUSB2E22EVM-CAT schematic pad C3 is connected via SW2 switch
what is the purpose of this SW2 switch?
is it allow to short this pin to GND?
Thanks
Tamir
Part Number: TUSB2E22 Hello Guys,
Good day.
For RESETB pin(E4) of TUSB2E22 eUSB2-USB 2.0 Dual Repeater, do we need pull-up resistor?
Datasheet shows this is not an option but the schematic for the TUSB2E22EVM-CAT shows the RESETB pulled up to 1.8V_IO.
…
Part Number: TUSB2E22 Hello TI support team,
Based on spec, given that register access protocol (RAP) is optional, it is the system architecture and implementation to ensure if RAP is required
We are developing our eUSB2, we would like to know RAP is…
Other Parts Discussed in Thread: TUSB2E22 Hi Experts,
Good day. I came to this forum with reference to my previous post: SN74AXCH1T45: Data rate query
Based on our interaction there with an experts, the client responded as follows:
"But the problem is we…