Part Number: SK-TDA4VM Hi Team,
I have found some git lfs files in the tiovx of RTOS SDK(8.1). Please suggest a way to pull them or does it get fixed/pulled during the "make sdk" ?
Please find the details of the lfs files below.
The test data…
Hi Karan,
Thank you for the Debug session. I removed the gpio hog part from my device tree and now I see all four CAN probe in dmesg.
root@j7-evm:~# dmesg | grep can
[ 3.720273] davinci_mdio 46000f00.mdio: no live phy, scanning all
[ 4.196886…
Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 , Hei,
I am testing the TUSB320EVM in DRP mode. For instance I try to source power to a phone over the USB-C for charging (input power to the EVM comes from the USB micro B with 5V/2A at least…
Part Number: TDA4VM Other Parts Discussed in Thread: TDA4VH hello,
I am using TDA4VH EVM board,and i‘m using sdk8.5.
I compiled OPTEE_OS according to the method in the figure below, and got tee-pager_v2.bin。
then i make the uboot,i change the Makefile…
Part Number: TDA4VM Hi everybody ,
I would like to perform boot of the J7 EVM using U-Boot on MCU R5 (tiboot3.bin) and U-Boot on Main A72 (tispl.bin) from the PSDK-LA 7.0 release to run QNX SDP 7.0 on the A72 and Autosar on MCU R5.
Specifically we want…
Part Number: TMDS64GPEVM Hi
We are using TMDS64GPEVM board. We have issues with NOR memory... Is there a some problem with driver?
We are using processor_sdk_linux_am64x_07_03_00_02 SDK
These are commands and outputs
root@am64xx-evm:~/sh# cat /proc/mt…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X Tool/software: TI C/C++ Compiler hi Champs:
I have a small question:
To prepare a Sitara Linux with pre-built image is simple. Just to trigger a script : ./create-sdcard.sh.
But the TDA4 has no such a simple way…
Carlos, TUSB320 can be configured over GPIO or I2C. Please see the TUSB320EVM on ti.com (link below). If customer wants a simple method for configuring the EVM they can use the DIP switches on the EVM. TUSB320 I2C interface can be used with most general…
Booting from eMMC
Intention will be to flash the boot0 partition with R5 SPL, A72 SPL, A72 u-boot and sysfw.itb and then flash the user partition with a tiny file system.
We use tiny fs right now as the full file system will take a lot of time to…
Hi David,
Could you also measure the CC1/2 voltages when the PC is connected? The EVM seems to be configured correctly so you should see a voltage greater than 250 mV. this signals that a Type-C connection has been made. Other things to confirm:
Measure…