Part Number: TUSB322I Other Parts Discussed in Thread: TUSB322 , TUSB320 Hi experts,
I have 2 questions. If am using the TUSB322I on a prototype on the I2C bus.
1. May I ask what is the proper way to detect attach and detach of the USB C port using this…
Hi Justin,
Thanks for your quick reply! I will try the LRPD demo.
I've read the 0753.swru546c----mmWaveICBoost and Antenna Module.pdf , in which it mentioned " IWR6843ISK / IWR6843ISK-ODS (deprecated)". I want to ask what the "deprecated" means…
Part Number: AM3354
Hi!
Customer own board:Based on an335x_evm and am335x_evmsk SDK: PROCESSOR-SDK-LINUX-AM335X 06_03_00_106
It is modified in DTS
matrix_keypad: matrix_keypad@0 {
compatible = "gpio-matrix-keypad";
…
Hi Alex,
For my connections Ch2 = LA-RA and Ch3 = LL-RA according to the lead derivation.
You are correct. I am using LA, RA ,LL and RL only.
I noticed that in the schematic of EVM (page 53 of ADS1198ECG-FE Datasheet ) for some reason the bandwidth of…
One difference between the TUSB320 and the TUSB320LAI is the addition of Accessory Mode (audio and debug) when configured as UFP. The TUSB320LAI supports this feature while the TUSB320 doesn't. Refer to Table 1 in datasheets. This feature is enabled…
Part Number: ADS1292ECG-FE Hi
How to modify the ADS1292ECG-FE EVM to support two channel ECG ?
one channel for LEAD I (LA-RA),another one channel for LEAD II (LL-RA) .
We are referring to the schematics of ADS1x9xECG-FE Demonstration Kit P51, extracted…
Hi Team,
We are trying to Build AGL OS for TI Jacinto 7 platform.
But the build is getting failed due to below errors:
Summary: 3 tasks failed:
ERROR: Task (/home/ssdrive/AGL_TOP/needlefish/external/poky/meta/recipes-devtools/quilt/quilt-native_0.67.bb…
Hi Team,
We are trying to Build AGL OS for TI Jacinto 7 platform.
But the build is getting failed due to below errors:
Summary: 3 tasks failed:
ERROR: Task (/home/ssdrive/AGL_TOP/needlefish/external/poky/meta/recipes-devtools/quilt/quilt-native_0.67.bb…
Hi Karan,
Thank you for the detailed response. Will try to answer your questions below
1) I wanted to understand your setup, can you please comment if you are running on the TI EVM and also on what SDK release are you latched on to?
I am using SDK…
Hi Vishal,
I see only 2 GPIOCHIP for main domain GPIO 1 & 2. We are using wkupdomain GPIO0_4 and main domain GPIO6 to blink the LED. In device tree i see pinconfig for both added.
root@j7-evm:~# find /proc/device-tree/__symbols__/ | grep gpio /proc…