Hello LGE Engineer,
Were you able to resolve your connection issue? I did see some internal traffic where your group was OKed to get the necessary collaterals. Also, it appears that you all may have needed to update a legacy adaptor.
To expand: The recommended…
Hello Ahmed,
Thanks for the updates.
Originally this question was about the difference is noise performance between the two PACE amplifiers. For that, our design team ran some CMRR simulations to analyze the distribution in CMRR performance. Based on…
Part Number: ADS1298
Hello,
I am playing with EVM ADS1298RECGFE-PDK with channels assignment as follows: LA = IN2P; RA = IN2N, IN3N; LL = IN3P; C1 = IN8P; N = ECG_RL. I use unipolar 2.5V supply voltage. Which bits from RLD_SENSP and RLD_SENSN registers…
Dear Margarita,
I did remove all our changes and now I can see the device as per your list. root@am57xx-evm:/mnt# ls -la /lib/firmware/dra7-ipu2 fw.xem4 lrwxrwxrwx 1 root root 40 Jul 19 2019 /lib/firmware/dra7-ipu2-fw.xem4 -> /lib/firmware/dra7-ipu2-fw…
Part Number: TDA4VM Hello,
on our custom board we have an ASIC which is configurable via SPI (SPI Slave).
This ASIC is connected to MCSPI0
Ball TDA4
AA1 SPI0_CLK
Y4 SPI0_CS1
AB5 SPI0_D0
AA3 SPI0_D1
We currently use a modified SDK version 06_01_00_05…
Hi Gibbs,
I would suggest try to boot to kernel using a tiny file system.
1. Create the tisdk-tiny-image.tar.xz (You can take the attached tar ball I generated and skip to Step2)
git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
cd…
Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 Hi,
I am using TUSB320EVM for testing purpose. Please let me know the method to configure CSR registers of TUSB320 IC when EVM is connected to PC through microAB port J6 via USB-A to Micro…
Hi Nathan,
Yes this is a bug. You can use the below information to address the issue.
I have attached the patched (same as in https://e2e.ti.com/support/processors/f/791/t/924900 ) and the built sysfw.itb.patched from my setup. Rename the sysfw.itb.patched…
Hi Tomitama,
I do not have a am65xx EVM handy but I haven't validated the instructions - but they should work for you.
So as I understand that you have the boot0 partition of the eMMC flashed and now we are looking at flashing the file system to the…