ti-linux-kernel6.8-error.txt
Hi TI engineers, I have uploaded linux boot dmesg here. please help. (about ti-linux-kernel 6.8 : the "memory reserved" of dts is wrong which need a benchmark or baseline).
Part Number: TUSB320 Other Parts Discussed in Thread: TPS25750 , USB-PD-CHG-EVM-01 Hi,
In my design I have just one USB 1.1 Host-Lite port available and needs external power source (5V, 3A).
Considering this I'm exploring if there's a way to using USB…
Hi Nick,
Here is the output (in AM62A3-Q1)
root@am62axx-evm:~# ls -la /lib/firmware/
total 10080
drwxr-xr-x 6 root root 4096 Mar 9 2018 .
drwxr-xr-x 10 root root 4096 Mar 9 2018 ..
lrwxrwxrwx 1 root root 58 Mar 9 2018 am62a-c71_0…
Good morning!!!
Thanks for your response. Previously, I loaded the default image using SDK v9.x, but now I'm using our custom image with the latest SDK v10.0, and the error has been resolved.
In the previous setup, I used the default image and…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: MMWCAS-DSP-EVM ,
Hi Team,
we are trying to connect the system MMWCAS-RF-EVM + MMWCAS-DSP-EVM to the computer for evaluation and we are obtaining the following error:
[17:06:46] Matlab Runtime…
Hi,
1. I still don't see the explanation/clarification what does ICG mean?
2. Do they happen to have/use a ADS1298R evaluation kit/board(EVM)? Has customer had/used an evaluation kit/board(EVM) to do the tests they want to do? It's suggested to do …
Part Number: TPS65987EVM This post will be involving a few questions about the EVM and final implementation of the TPS65987DDH for our customer. Problem #1: The EVM the communications via I2C over the FTDI bridge are unreliable at best. The current problem…
Neil,
Thanks for the confirmation, I was wondering how effective pulls become 0.9k. Yes checking with the Oscilloscope provides better voltage resolution.
Do you have any other board/interfaces connected to the EVM? While probing on the scope it's good…
Hello La,
You can use an electronic load or resistive load that draws enough current.
TI provides an EVM for testing purposes. The EVM document is here https://www.ti.com/lit/ug/sluu273/sluu273.pdf
This will help you understand the connections and process…
Hi,
May I ask what lead or electrode do you intend to use/read in Channel 3? Precordial leads or Which V#?
And, Are you using a ECG simulator? Does that ECG simulator have function/capability to support the electrode or lead you want to input to Channel…