Hi Michael-san, I found TUSB320-LA-EVM uses 1Mohm (±1%) at the moment. http://www.tij.co.jp/jp/lit/ug/sllu235/sllu235.pdf It is ideal for my customer if is acceptable.. Could you confirm once again if 1Mohm is acceptable or not? Best Regards, Yaita
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: SK-TDA4VM Hi team,
When I run cameras with FRAKA (DS962 & DS953) a while time(7hours), the display and system will stuck.
my gstearmer pipeline:
gst-launch-1.0 \
v4l2src device=/dev/video-tevs…
Hi,
TI doesn't provide the time delay info as it could depends various settings(e.g. clock, SPS, SCLK, etc) and the GUI doesn't probability as there are OS and several applications and software in between.
Note- even on chip time delay it also…
Hi,
May I ask where do you see " with output data rate of 1024Hz, the noise level should be around 3.9μVPP. " ? I don't see such entry in the Tables.
What device and how did you measure the noise on human body?
Do you happen to have/use…
Part Number: TDA4VM Dear Team ,
We are going to stat porting activity with TDA4x EVM for the same we planning to use R5F core on TI-RTOS OS, so for debugging purpose which debugger device we can use, can it be done using XDS560V2 or we need use Lauterbach…
Danh Doan said: I checked Bus I2C1(main domain) are already define in device tree, and omap_i2c_probe function not called.
I am using the latest 8.6 SDK. Here is the log on the TI EVM: root@j7-evm:/sys/bus/i2c/devices# ls -la
total 0
drwxr-xr-x 2 root…
Part Number: SK-TDA4VM Hello team,
Customer still has some outstanding questions on the SDK. Please refer below. Thanks!
~~~~~~~~~~~~~~~~~
In the plain untarred ti_rtos SDK I see several file in this particular folder which gets deleted when I run a …
Hi Malik, hi all
Let me provide some links that might be helpful to implement a solution:
www.ti.com/.../TIDA-01602 Barrel Jack to USB C PD and USB Type-A to USB Type-C TIkit Reference Design
www.ti.com/.../BQ24392 SPST USB 2.0 High-Speed Switch With…
Hi,
According to the data sheet and ECG concepts -
I.e. without using RLD, people may encounter more noise, and may need to do further analog signal conditioning and/or DSP to meet the product's needs, but it all depends on the applications and product…
Part Number: TDA4VM
bHello, i downloaded the latest linux sdk from here : PROCESSOR-SDK-LINUX-J721E_07.03.00.05 | TI.com . Then I tried to use /bin/mksdboot.sh to create a bootable SD card as said here : 1.1.3. Formatting SD card on Linux — Processor SDK…