Part Number: TUSB5461-Q1 Other Parts Discussed in Thread: TPS65987D Hi exports,
have post a new thread, the link is TDA4VH-Q1: Configuration of the device tree related to TUSB5461-Q1 and TPS65987D - Processors forum - Processors - TI E2E support forums…
Part Number: TUSB5461-Q1 Other Parts Discussed in Thread: TUSB8041 , HD3SS6126 Hi All,
Can I use TUSB5461RGFRQ1 to split all USB data lines (USB2 & 3) into two.
I do not need DP 2.1 alt mode.
As I need to drive HD3SS6126 downstream then into TUSB8041…
Hi BoWen,
Apologies for the delay.
BoWen Zhang said: 1. Why is the VBUS voltage of the TPS65987D 0 when I connect the display screen via Type-C? Is it necessary to configure the TPS65987D?
2. If configuration is needed, how should I configure the…
Part Number: TUSB5461-Q1 Other Parts Discussed in Thread: TUSB564 Tool/software:
Regarding TUSB546 & TUSB564 CC pin FLIP & NON FLIP, I am curious as shown in the following picture. 1. CC1 (TUSB546) -> CC1 (TUSB564) : NON FLIP 2. CC2 (TUSB546) -> CC2…
Part Number: TUSB5461-Q1 Other Parts Discussed in Thread: TUSB1146 , TUSB1044A Tool/software: We are wanting to design a test board for automotive USB hubs using an active redriver/mux that can be used in two different setups. The first would be used…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TUSB5461-Q1 , TDA4VH Tool/software: Dear all
I am currently using TUSB5461-Q1 to receive the dp signal from serdes and output it to the Type-C interface, but I have no idea how to modify the device…
Part Number: TUSB1064 Other Parts Discussed in Thread: TUSB1146 , TUSB5461-Q1 Hi
We are trying to change DP EQ setting by I2C, it works, but I found it seems that we have to plug out then plug in the USB-C to make it work. We want the EQ adjustment…
Part Number: TPS25763-Q1 Other Parts Discussed in Thread: TUSB5461-Q1 Tool/software: Is it possible to use TPS25763-Q1 to implement a Type-C port in DFP configuration with USB3+PD and DisplayPort as source?
Planned setup: CPU/GPU would provide USB2…
Hi,
Yes the TUSB5461-Q1 EVM can be used here. However, keep in mind that TUSB5461-Q1 is nothing more than an active mux.
You will need an external DP source + USB host to test fully test the EVM.