Part Number: TVP5150A Hello Team,
PN#TVP5150AM1IPBS
We have received a request from our customer to submit delivery specifications.
We need to include ESD-HBM and CDM test results, but the datasheet and TI.com did not include ESD-HBM and CDM test results…
Part Number: TVP5150AM1-EP Other Parts Discussed in Thread: TVP5150A Hi Team,
The customer is using TVP5150A. The customer sets the 640*480 resolution and the screen is fine. And the circuit can work properly. But when he sets 800*600 resolution, the screen…
Other Parts Discussed in Thread: TVP5150AM1 , TVP5150A Hi all,
May I know the differentiations on TVP5150MEP, TVP5150A and TVP5150AM1?
The default code could initialize below marking.
But could not initialize following marking.
If I change the part…
Other Parts Discussed in Thread: TVP5150A , TVP5150AM1 , TVP5150 Hi,
I with the TVP5150A recieve CVBS signal, and the Imx515 CPU to process the ITU656 data. But the image is not clear, the colour of the image is not right and the image to bicker.
I have…
Part Number: TVP5150AM1-EP Other Parts Discussed in Thread: TVP5150A What is the maximum resolution supported b TVP5150AM1-EP??
Will it support 720x576 resolution(standard PAL resolution)
[In datasheet, active pixels per line alone is menionted as 720…
When you are using 'ITU-R BT.656' does not require the use of the discrete synchronization signals on pins VSYNC, HSYNC, FID, AVID. These discrete synchronization signals can optionally be enabled and connected for applications requiring them. …
Mickey,
High Rel only offers the TVP5150A for decoder.
I have communicated with one of the decoder experts, and he indicated that the 5150 covers nearly all of the standard resolutions.
If you have more details on requirements, possibly he can guide…
Part Number: TVP5150AM1 Other Parts Discussed in Thread: TVP5150A Hello,
Regarding to the monochrome video(CVBS) input with no color burst on TVP5150AM1, my customer is asking some question.
They are using this device for security camera option product…
Dear Steve,
Here are the answers to your questions.
Q1. Are you able to completely disconnect from the Altera just to make sure there is not some strange back current of something else related to the Altera?
A1. No, we can't disconnect the FPGA, the…