Part Number: TVS1801 Tool/software: Hi team,
I put TVS1801 as a lightning surge protection component for IEC61000-4-5. When 0.4kV was applied, it broke in short mode. If it broke in short mode, can you assume what kind of load was applied to the device…
Part Number: TVS1801 Other Parts Discussed in Thread: TCAN332 , Hi Sirs,
We have use TI TCAN332 and we would like survey ESD protect on CANH、CANL .
Does TVS1801 is suitable solution?
TCAN332 specification 8.1 mentions that the maximum can withstand…
Hi Mitchell,
TVS1800 is a unidirectional device, so if your application requires negative signals, it would clamp those negative sections and kill the signal.
If you like the performance of TVS1800, we have TVS1801 which is bidirectional and offers…
Hello Inho,
Unfortunately, we do not have any devices with an 18 V Vrwm who's primary function is ESD suppression. However, you could protect the 18 V power line to the amp from surge using a TVS1801, if you don't have a surge protection device already…
Part Number: TPD1E10B06 Other Parts Discussed in Thread: TPS25947 , TPS25947EVM , TVS1801 , TVS1800 , TVS2200 Hi, TI expert
The customer company has a question about selecting a TVS device with a surge function.
Q1) Can I confirm what level the TPD1E10B06…
Part Number: UCC39002 Other Parts Discussed in Thread: TVS1801 Hi Team,
My customer is designing the UCC39002 application, asks us about ESD protection for LS pin of UCC39002. In case of their system, one power board has one UCC39002, and LS pins of…
Hello Hao,
Thank you for your reply.
I understand clamp voltage is around 17V.
I have another question.
TI has flat clamp surge protection device which is based on FET solution. (like TVS1801)
In THVD1429, Is this TVS solution same as FET…
Hello John,
you can take a look at the TV1801 surge protection device to prevent Vbat input voltages above 18V :
http://www.ti.com/product/TVS1801
In addition there is a training video "How to Design Protection Circuits for Analog I/O Modules" …
Other Parts Discussed in Thread: ULN2003B , TVS0500 , TVS2200 Hi,
Good Day. I would like to confirm if the devices below can support 230V AC line surge protection for PWM Power Supply Unit.
https://www.ti.com/product/TVS1801
https://www.ti.com/product…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…