Part Number: TWL1200-Q1 Other Parts Discussed in Thread: TWL1200 Hi Team.
The IBIS Model of TWL1200 is only for BGA available. Could you also provide the IBIS Model of TWL1200-Q1 in TQFP Package?
Many Thanks,
Stefan
Part Number: SN74AVCA406 Other Parts Discussed in Thread: TXS0206A , TWL1200-Q1 , TXS0206-29 , TWL1200 , TXS0206 , TXS02612 Hello support member
# SN74AVCA406 MAX Clock speed
Checking the data sheet of SN74AVCA406, the MIN of Clock seems to be 52MHz.
Q1. …
Part Number: TWL1200-Q1 Other Parts Discussed in Thread: AM4376 , TWL1200 , WL1837MOD
Hi,
We are looking to interface the WL1837MOD which has 1.8V SDIO lines to our 3.3V IO lines on the AM4376 . Looking on page 4 of this report for level shifting the WL18…
Part Number: TWL1200-Q1 Other Parts Discussed in Thread: TXS02612 , , TWL1200 I have an application where I need the SDIO output signals to all be floating or with weak pull-ups when the input is the same. At first I wanted to use TXS02612 along with the…
Part Number: TWL1200-Q1 Hi,
We are looking to interface the WL1837MOD which has 1.8V SDIO lines to our 3.3V IO lines on the AM4376 . Looking on page 4 of this report for level shifting the WL1837MOD IOs: http://www.ti.com/lit/an/swra448a/swra448a.pdf , I see…
Other Parts Discussed in Thread: TWL1200-Q1 , TWL1200 Dear support team
My customer found the level of TWL1200-Q1 output falls (see attached file)
(1)Could you advice about cause of this and solution?
(2) I guess parasitic capacitance of output side is…
Dear All
Could you advice about attached schematic? I am worried about two points of follows. ・ The B side is not SoC in conformity with Wi-Link-6. ・ Unused pin is Open. (If it need Pull Up/Down,please let me know)
Thanks
Best Regards
Tomohiro Nagasaw…
Could you please tell me if TWL1200-Q1 has EOL plan in next 3 years?
or other new device to instead of TWL1200?
My customer was using TWL1200(BGI -package) which will be EOL.
So they want to change to TWL1200-Q1.
They are worrying about if TWL1200-Q1…
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum
FET R…
Hi,
I am able to probe the WLAN with mmc4.
Did the following changes,
1) Manually enabled the WLAN_EN on TWL1200-Q1.
2) Did the following changes on dts file (dra7-evm.dts),
&mmc4 {
max-frequency = <1000000>;
wlcore: wlcore@2 {
…