Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0104 Hi team,
My customer is using TXB0104 to convert 3.3V SPI to 5V SPI signal. They found some interference on MOSI signal from 1MhZ CLK signal. You can find the waveform as below.
Yellow…
Part Number: TXB0104
Tool/software:
I need a level shifter to converter the Low Power Mode signal of MIPI DSI (1.2V at 10Mhz) to 2V or more is TXB0104 up to the task? and what other options do I have?
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0202 Tool/software: Hello, im having issue with this component, basically im using this component as voltage translator and it works fine for like some hours and after a while it breaks, i saw that…
Part Number: TXB0104 Tool/software: Hi Team,
I know we don't have TXB0104 Pspice model but want to check which similar device have Pspice model and can help evaluate TXB0104 ?
Thanks.
Part Number: TXB0104 Tool/software: Hello,
I am using TXB0104 for voltage level translation of I/O between two microcontrollers operating at 3.3V and 3.0V. Are there any output source-series termination recommendations to maintain trace impedance of…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0104 Tool/software: Hi,
I am using the TXB0104 in my design (schematic attached. in my design VCCB is 5V and VCCA is 3.3V - The input to VCCB is off / 24V fed to the pins via resistor split…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0104 , , TXU0104-Q1 , TXU0204-Q1 , TXU0304-Q1 Tool/software: I'm trying to design a 1.8V to 3.3V circuit.,When the PCB was finished I realized that this feature was not available,Because the…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 TXB104RUT We're having a SPI speed problem translated over the TXB104RUT. Mostly due to the propagation delay on the slave side (16-20 ns, though rated for max speed of 24 MHz). So far 8MHz…
Part Number: TXB0104 Tool/software: Data sheet is a bit confusing does the OE pin require and external drive source? Some verbiage in DS makes it sound like it does but other times seems not, here is one example:
the OE pin only has a pull down…