Part Number: TXB0104 Hi
We are using TXB0104RUTR voltage translator in the design to convert 1 wire DQ signal from 3.3V to 1.8V. This design did not work for us we are not getting correct data from this signal. After reading the datasheet came to know…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 Tool/software: Hello,
In my system I need to scale down SPI signal and TXB0104 seems to be ticking a lot of boxes, including cost. The caveat here is that it needs to do it in almost back…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0104 Hello Team,
On customer behalf I have a short question related to Vola specification from datasheet of TXB0104-Q1. On page 6, we have the following:
Can you please review and comment…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: LSF0204-Q1 , TXS0104E-Q1 I need a level translator which translates from 3.3V-1.8V (vice-versa also). Please suggest a suitable Level translator.
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0104 , SN74LVC3G17 , TXS0104E Tool/software: Hi team,
customer use TXB0104 for 5V to 3.3V level shift. The input signal is from optocoupler encoder and it's a open drain signal. I know that TXB0104…
Part Number: LSF0204 Other Parts Discussed in Thread: TXB0104 , Tool/software: Hello,
There are lot of confusions regarding the pull up resistor limitations of both LSF0204 & TXB0104 bidirectional bus switch & level translator respectively.
Comparatively…
Part Number: TXB0104 Tool/software: Hi Team,
Use TXB0104 as redriver
CPU signal cannot be pulled down
The circuit design is as follows
Cable length 100cm
Or suggest an IC suitable for this circuit
Thanks
Part Number: TXB0104 Tool/software: VCCA = 1.8 Vdc VCCB = 5.0 Vdc the datasheet does not provide details on how the IC decides which direction to transmit the data. Pin 3, A2 Good board waveform (on left). Bad board waveform (on right)
Part Number: TXB0104 Tool/software: Hi,
I am looking for a level shifter (preferable a quad-signal one) which includes isolation.
Low side voltage: 1.2V
High voltage side: 3.3V or 5V
bit rate: >80Mb/s
Is may you please recommend me a part…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 , TXU0202 Hello.
I want to use TXB0104 AS SPI BUS LEVEL SHIFTING/TRANSLATOR 5V TO 3.3V.
I also will need RX TX (UART COMMUNICATION) TRANSLATOR 5V TO 3.3V IN THE SAME PCB.
I want to use…