Other Parts Discussed in Thread: TXB0106-Q1 , TXB0302 , TXB0304 , TXB0106 Hello Team,
can our TXB0106-Q1 used for QSPI @ 64MHz?
Application is a 5V micro controller interfacing a QSPI Flash with 3.3V.
Thanks
Josef
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXB0106-Q1 , Hi team,
When does it operate as Open-drain or push-pull output operation? How could we configure its output as push-pull?
I would like to use it as push-pull output but I cannot find…
Thank you for your kindly reply!
My customer has some follow-up questions:
1. Why can't I²C signals use COMS? What happens if I use COMS?
2. Could you help me choose the product with automotive regulation?
I've seen three of the automotive…
Part Number: TIC12400EVM-KIT Other Parts Discussed in Thread: TIC12400 , TXB0106 , TIC12400-Q1 Hi I am new with MSDI & trying to interface TIC12400Q1 EVM SPI Communication with External Microcontroller(NXP: S32K118) So i am transmitting 0x02000000 (DEVICE_ID…
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum
FET R…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXB0106-Q1 , , TXB0104-Q1 , TXB0106 , LSF0108 Hi,
Customer would like to using level translation for SPI 1.8V to 3.3V in automotive.
TXB0106-Q1 is considered but 125C operating condition is needed…
Other Parts Discussed in Thread: TXB0106-Q1 The operating free-air temperature range of TXB0106-Q1 is –40°C to 85°C, and its rating is Automative. Why?
In my original oponion, the difference between Industive and Automative is Temperature…
Fig1 question
This wave pattern rises 260mV from GND, but why will be?
Is there the method to improve 260mV?
Fig2 question
Why will it fall 110mV?
Fig3 question
1ch:Lo fixation
A wave pattern of ch2 does crosstalk in 1ch, but why will be?
Other Parts Discussed in Thread: TXS0104E-Q1 , TXB0104-Q1 , TXB0106 Would TXB0106PWR pass the following ESD tests on port B?
ISO 10605; 8kV contact 330pF/2k
ISO 10605; 15kV air 330pF/2k
Best Regards
Henrik Danielsson
Other Parts Discussed in Thread: OPA890 , CD4066B , SN74LV595A-Q1 , TXB0106 Hello
Could you please recomend a latch or shift register to take and hold data from an MPS430 device sent to the control pins of a CD4066B device? The switch input is a low level…