Part Number: TXB0304 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 The internal circuit output of the TXB0304 chip needs to pass through a 1K resistor, which will cause a resistor-impedance mismatch during high-speed signal conversion,…
Other Parts Discussed in Thread: TXB0304 , TXB0104
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters >> Current FAQ
The most common reason is due to impedance mismatches.
TXB0304 specifies a stronger output impedance than TXB0104…
Part Number: TXB0304 Other Parts Discussed in Thread: TXU0304 Hi,
We are using TXB0304RUTR bidirectional level translator in our design for converting 3.3V to 1.8V. Can you please confirm the supply range for VCCA and VCCB.
We need to establish connection…
Part Number: TXB0304 Hi team,
Does "disable" below mean high-z status on input/outpout ports?
Could you please share the true table in all conditions?
Nison
Part Number: TXB0304 Other Parts Discussed in Thread: TXB0104 , TXU0304 , TXU0104 , TXU0204 , TXS0108E , SN74LXC8T245 We want to use TXB0304 to transfer 30Mhz CLK from 3V3 to 1V8. Owing to the trace at the output is too long(about 7000mil) , we found…
Part Number: TXB0304 Other Parts Discussed in Thread: TXU0304 , TXB0104 Hello Team,
We use the SPI trace length is about 20" on MB, we plan to add a SPI buffer on MB
Can the TXB0304 be used as a buffer for SPI? or do you have any better suggestions…
Part Number: TXB0304 Other Parts Discussed in Thread: TMUX1511 , SN74CBTLV3126 , SN74LV125A Tool/software: Hi, Sir,
We have a motherboard (CPU: Intel Core i5-1335UE) that uses the TXB0304RSVR as a level shifter to convert SPI from 3.3V standby power…
Part Number: TXB0304
We use TXB0304 to transfer 33MHz and 16MHz CLK from 1V8 to 3V3.
The topology list show as below:
Topology 1: QSPI 16MHz trace length is 14" after level-shift, the waveform of CLK can't be recognized.
Is there any solution…
Other Parts Discussed in Thread: TXB0304 Hi team,
is there any level shifter recomendation for the Quad-SPI application?
Reqiurment:
Max Clock: 100Mhz
1.8V to 3.3V/ auto-bi-directional
and Host CPU SPI spec TCLH (clock high time)/ TCLL (clock…