Part Number: TXB0604 Other Parts Discussed in Thread: TXB0104
Hello TI Support Team,
We are looking for an auto-bidirectional line redriver for an eSPI interface between an AMD CPU/PCH and a Super I/O device.
Application conditions:
eSPI_IO…
Part Number: TXB0604 Hello,
I would like to clarify whether the TXB0604 is suitable for I²S level translation between two voltage domains in an audio application.
Interface:
I²S audio at 48 kHz, 24-bit
Point-to-point connection, short…
Part Number: TXB0604 Hi Team, Previously i have asked for the MIPI RFFE Level translator suggestion an you have suggested the Biderectional part TXB0604RUTR, please refer the below mentioned link for the thread https://e2e.ti.com/support/logic-group/logic…
Part Number: TXB0604 Other Parts Discussed in Thread: TXB0606 , What is the recommendation for unused A/B channels on the TXB0604 or TXB0606. The datasheet does not cover whether to connect unsued pins to GND/VCC or leave as NC.
Thanks
Part Number: TXB0604
Hi
I noticed that the TXB0604 datasheet does not include the RGY (VQFN-14) package drawing or example board layout / recommended land pattern information.
Could you please provide the RGY package drawing PDF and the recommended…
Part Number: TXB0304 Other Parts Discussed in Thread: TXB0604 , TXU0304 Hi TI experts
We design SPI level shifter with TXB0304, however, the infoamtion from TI web site recommend TXB0604 for drop-in placement.
May we know any spec difference/improvement…
Part Number: TXS0108E Other Parts Discussed in Thread: TXB0604 I want to confirm if the TXS0108E can be used on the level shift supporting the I2C(400kHz) and SPI(10MHz). The A side is 1.8V and the B side is 3.3V. Based on this condition, what is max…
Part Number: TXU0104 Other Parts Discussed in Thread: TXB0604 , SN74AXC4T774 Hi team,
Customer is evaluating TXU0104 in their wearable application.
They find there is the power consumption data under normal condition.
They also care alot about the…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXB0604 Deat TI experts,
My customer made their PCB using TXB0104-Q1 for SWD(Serial Wire Debug) interface.
During the test, customer found that SWD is not connected properly even waveform seems…
Part Number: TXB0606 Other Parts Discussed in Thread: TXB0604 Hi,
We are looking at using TI’s TXB0606 Auto-Bidirectional Level translator for a QSPI interface that is cabled off board from our processor. This app note make it seem promising for this…