Part Number: TXS0206 Tool/software: Hi, I've designed in the TXS0206, but notice there is a TXS0206A version as well, data sheet is newer, but don't detect a difference in spec sheets. Seems both are available, neither shoiw EOL.Are they totally compatible…
Part Number: TXS0206 Hello team,
I need a level shifter for my SDIO-Interface (SDR25 or faster). The master must be powered at 3.3V. The slave can only be powered at 1.8V. Which level shifter would you recommend?
AEC-Q is not required. 85°C should…
Part Number: TXS0206 Tool/software: Hello,
I'm using TXS0206YFPR SD card voltage translator in my project and I wonder if I can swap DATA,CLK and CMD lines for more convenient routing.
Device pinout determines fixed pins for DATA3..0, CLK and CMD…
Part Number: TXS0206 Other Parts Discussed in Thread: TXS0108E , Tool/software: i t is mentioned in the data sheet that the component ±8-kV Contact Discharge IEC 61000-4-2 ESD, can I assume it supports ±15-kV air discharge as well?
Thanks,
Dori
Part Number: TXS0206 Other Parts Discussed in Thread: TXS0108E I'm considering using the TXS0206 in an application to interface an Intel Stratix 10 FPGA with 1.8V I/O to a 3.3V SD Card Interface. I'm struggling to understand the TXS0206 Vih and Vil specs…
Part Number: TXS0206 Hi,
We are using SD card connector GTFH08131YHR in our design which is of 5V and has 8 positions, as our FPGA supports only 1.8V we need a level translator for this. Kindly suggest a level translator suitable for this connector…
Part Number: TXS0206 Hi,
When driving SD cards with VCCA=3.3V and VCCB=1.8V, is it safe to assume that the TXS206 specs can support up to DDR50?
Best regards,
Jumpei
Part Number: TXS0206 Other Parts Discussed in Thread: SN74AXC2T45 Hi,
I actually have several questions about the TXS0206 and TXS0206-029 . I am new to SD interfaces and after checking the support threads I didn't really find what I was looking for…
Part Number: TXS0206 Hello,
I want to use the TXS0206 device at full speed. Can you please provide me with the current consumption of the device itself - separetely on the VCCa and VCCb line with VCCa=VCCb=3.3 V I can not find those numbers in the datasheet…