Part Number: TXS02612 Other Parts Discussed in Thread: TXS0206A Hello,
I am considering TXS02612 to interface SD/MMC card with FPGA.
My FPGA IO works as 1.8V and the fact is SD/MMC card will operate at 3.3V
Therefore, I am considering TXS02612 …
Part Number: TXS02612 I am using the TXS02612 level translator in my design and would like to use the SEL pin as an enable control driven by a microcontroller GPIO.Is this approach considered reliable and feasible in a practical design? Also can you review…
Part Number: TXS02612 Hi,
We are planning to use the TXS02612 Mux switch for JTAG in our design. Instead of routing the clock signal to the dedicated CLK pin, we are planning to use one of the data lines (D0–D5) for the clock connection.
Could you…
Part Number: TXS02612 Tool/software: Hello TI Team,
I have a design based on TXS02612RTWR
I use only one port of it and second it un-used.
What kind of termination should I be providing for un-used port. Can I leave it open?
below is schematics…
Part Number: TXS02612 Hello guys,
One of my customers is considering using TXS02612 for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. They want to do the following things. 1. Signal…
Part Number: TXS02612 Hi, we are planning to use TXS02612 switch voltage level translator and we have reviewed the datasheet, but we are not able find the supporting speed of this part. Can you confirm the following questions below. 1. what is the min…
Part Number: TXS02612 Other Parts Discussed in Thread: TMUX1574 , AM6442 , TXS0206A Does TXS02612 support SD card High-Speed Mode?
When VCCA = 3.3 V and VCCB = 3.3 V: The propagation delay (tPD) of clock from controller to SD card (CLKA to CLKB) is…
Part Number: TXS02612 Hi Team,
We are using the TXS02612RTWR IBIS model for our simulations. While running the simulation from the B‑Port to the SD‑card connector, we are encountering a loading issue. Could you please provide your inputs/suggestions…
Part Number: TXS02612 Tool/software: Hi,
I am designing new hardware with Zynq 7000 SoC FPGA and interfacing SD Card via TXS02612RTWR. My question is: What is longevity of IC TXS02612RTWR from year 2025?
Thanks
Nandish Jasani.