Part Number: TXU0204-Q1 Hi team,
I have a question about the description in the datasheet P21 9.3.5 as below.
"It is recommended that the inputs are kept low before floating (disconnecting) either supply."
In my system, VCCA is active while…
Part Number: LSF0108-Q1 Other Parts Discussed in Thread: TXU0104-Q1 , , TXU0204-Q1 , TXU0304-Q1 Tool/software: ■Q uestion
① Does this model support I2S interface? ※I would like to confirm this as it is not mentioned in the datasheet.
② Can this model…
Part Number: TXU0204 Hi.
I have a question about output enable control of TXU0204.
My design is like below.
- VCCA=3.3V(Fixed), VCCB= 1.8V or 3.3V(Default)
- Output Enable referenced to VCCA through 10kohm resistor
From the link below Karan mentioned…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN74AVC4T245-Q1 , TXU0304-Q1 , TXU0104-Q1 , TXU0204-Q1 May I ask what are the differences between the previous SN74AVC4T245-Q1 and SN54SLC8T245 chips and the current TXB chips?
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN75173 , , SN74AHC125-Q1 , TXU0204-Q1 , TXU0304-Q1 Hello,
I have recently incorporated the TXB0104QPWRQ1 component into our design. Here is the circuit diagram. It essentially converts 5V to 3.3V. …
Two TXB I/Os must no be connected to each other. The outputs on both sides of the TXB are always active, and one output is not strong enough to override the voltage of the other one.
For unidirectional signals, you should use a unidirectional translator…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXU0304-Q1 , TXU0104-Q1 , TXU0204-Q1 Hi Team,
The Query is regarding TXB0104QRUTRQ1 Voltage Level translator ,
From datasheet VCCA<=VCCB (VCCA should not exceed VCCB)
Below Mentioning our design requirements…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: TXU0304-Q1 , TXU0104-Q1 , TXU0204-Q1 , SN74AXC4T245-Q1 , SN74AXC4T774-Q1 Hi, Support Team
as below diagram sky blue block, limited signal path as single direction.
Could recommend for level shifter…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 Hi we use your TXB0104 for our new ODM project design, our MCU control PSU(MCUoutput/PSU input) via TXB0104 level shift
(TXB0104 between MCU with PSU)
currently our customer…