Hello,
In addition to the recommendation above, there is a newly released device that is optimized for SPI buffering or level shifting:
https://www.ti.com/product/TXU0304
https://www.ti.com/product/TXU0304-Q1
It can support 1.1 to 5.5V supply…
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum…
You can use LSF, however, you would need external pullup resistors for translation. I hope you have the placeholder for those in the PCB.
In addition to the recommendation above, there is a newly released device that is optimized for SPI buffering…
Part Number: DRV3946-Q1 Other Parts Discussed in Thread: TXU0304 Tool/software: Hello TI,
Some time ago I requested access to the full datasheet of the DRV3946-Q1, but I haven't heard anything from it since. Could someone grant me access to this document…
Part Number: TXU0304 Other Parts Discussed in Thread: TXB0104 , SN74LV4T125-Q1 Hi Team,
Since customer need to select device which has P2P backup device, could you please kindly help to check if we have P2P device with TXU0304 and SN74LV4T125PWR? And…
Part Number: TXB0104 Other Parts Discussed in Thread: LSF0204 , TXS0104E , LSF0204-Q1 , TXU0304 Hello there,
You have few level shifters:
TXB0104, TXS0104, and LSF0204.
For TXB0104
7.3.2 Input Driver Requirements Typical IIN vs VIN characteristics…
Part Number: BQ75614-Q1 Other Parts Discussed in Thread: USB2ANY , TXU0304 Hello, I show the references connection in the AFE datasheet in this isolator is used. Can I directly connect or level shifter to the AFE RX & TX to the microcontroller.
Part Number: P82B715 Other Parts Discussed in Thread: TCA9803 , AFE4960P , SN74AXC4T774-Q1 , TXU0104 , TXU0304 Hi, I have a related question to the above case: Is this configuration possible, so the system can also act as level translating from 3.3V to…
Part Number: TLIN1021A-Q1 Other Parts Discussed in Thread: TXU0304 , TXU0202 , TXU0101 Hi,
We are using TLIN1021A-Q1 transceiver in our design for LIN interface. Our processor has 1.8V, lin interface is of 5V. Please suggest a level translator for lin…
Part Number: TXB0104 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 Hi we use your TXB0104 for our new ODM project design, our MCU control PSU(MCUoutput/PSU input) via TXB0104 level shift
(TXB0104 between MCU with PSU)
currently our…