Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050EVM-022 , UCC12050 , UCC33420 I am wanting to use the UCC12040 module for a noise-sensitive application. I require an synchronisable isolated regulator that produces low noise in the 500kHz…
Part Number: UCC12040 Other Parts Discussed in Thread: UCC33420 , I think to output +5.5V and -5.5V from one USB(+5V) bus power.
Since the UCC33420 is a fully isolated power supply, is it possible to generate ±5V by connecting one of the UCC33420 in…
Part Number: UCC12040 Tool/software: Hi,
We received chips, but they are incorrect. The packaging does say PUCC256602DDBR, but inside there are 25660 1 chips. Where we can get the correct chips? Needed soonest.
Can you please investigate? Order was…
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 , UCC12051-Q1 , UCC12041-Q1 Hi,
Am I correct in understanding that the difference between UCC12050 and UCC12040 is the insulation barrier (5kVRMS, 3kVrms), and that other electrical characteristics…
Part Number: UCC12040 Dear TECH. Support:
One question (see copy below), attached is the EVM board file of this device UCC12040deV for your easy reference.
this schematic below shows that there is C5 capacitance between primary and 2ndry side GND…
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 Tool/software: Hello,
some DC/DC converters, like UCC12040 and UCC12050 have recommended range for input voltage (Vinp) which is between 4.5 and 5.5 V. What would happen if input voltage…
Part Number: UCC12040 Other Parts Discussed in Thread: SN6505B , SN6505A Tool/software: Hi Team,
Can UCC12040 meet the below application conditions?
Vin 4.5~5.5V Vout 3.6V(1A 500mS) Ambient temperature -40~+85 degrees
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 , UCC33020 , UCC33420 , UCC15240-Q1 , UCC14140-Q1 , UCC14131-Q1 , UCC3808-2 Tool/software: Please recommend isolated DC/DC converters that is not a module power supply and has a withstand…