Part Number: UCC14131-Q1 Other Parts Discussed in Thread: UCC33421-Q1 Hi! I had a previous forum post marked as related to this post, but the thread got locked. Here is the repeated post text for reference:
"According to the datasheet of UCC14131QDWNRQ1…
Part Number: UCC14131-Q1-CALC Other Parts Discussed in Thread: UCC5881-Q1 hello Andy
Could you share me UCC5881-Q1: UCC5881 EMC SIMULATION spice model ?
Part Number: UCC14131-Q1 Hello. We are using the UCC14131 to drive a GIT GaN device. Immediately after starting GaN driving, the FBVEE pin exceeds 2.8 V with respect to the VEE reference, which causes an abnormal shutdown. We have confirmed the abnormal…
Part Number: UCC14131-Q1 Other Parts Discussed in Thread: UCC33421-Q1 , Hi! According to the datasheet of UCC14131QDWNRQ1, the minimum seconday side voltage supported by the device is 10V.
I have an application, where I would benefit greatly by reducing…
Part Number: TIDA-010210 Other Parts Discussed in Thread: UCC14131-Q1 Tool/software: Hello, In case we use UCC14131-Q1 instead of UCC14150DWNQ1 in the TIDA-010210-GaN reference design, do we still need to change the peripheral circuits? Thanks.
Part Number: UCC14131-Q1 Tool/software: Hi team,
For 5KVrms HiPot test, the distance b/w Primary-side and secondary-side need 15mm.
In customer board, the remain distance is only 11mm. Could you let us know what's recommendation on board design can…
Part Number: UCC14131-Q1 Tool/software: Hello,
are the Temperatures according to efficiency given in the datasheet Tjunction or Tambient ?
If the Efficiency is Junction Temperature are there any values for Tjunction 120°C available?
Thanks a…
Part Number: UCC14131-Q1 Other Parts Discussed in Thread: UCC5880-Q1 Tool/software: Device operates normally for approx 28ms whilst driving UCC5880-Q1 with 4 MOSFETs. Device was configured using TI spreadsheet.
Works normally without being connected…
Part Number: UCC14131-Q1 Tool/software: Vin=13v, Vfbvdd-Vee=2v4, Vfbee-Vee=2v4, case temperatures are cool to touch, so PG should be pulled low.
Vdd-Vee = 17v2 and COM-Vee=5v.
Part Number: UCC14131-Q1
Tool/software:
Dear TI support team,
I would like to request your assistance in reviewing the schematic for the design to ensure it is implemented correctly.
Thanks!