Part Number: UCC256404 Tool/software: Hi team
Burst soft ON doesn't work on UCC256404. Burst soft OFF works. This is true whether the load is light or heavy.
The settings are as follows: BMTH: 1.8V BMTL/BMTH ratio: Option 1
Lowering the BMTL/BMTH…
Part Number: UCC256404 Tool/software: Hi Manikanta and Team, what was the outcome of the above question? We have a similar problem with start up behaviour of UCC256404. BR, Leo
Part Number: UCC256404 Tool/software: Hi,
The junction temperature of UCC2564040 is -40°C. Can this IC work up to -55°C or the parts can be screen out to operate at -55°C.
Thanks
Ankit
Part Number: UCC256404 Tool/software: I have problem to start modified eval board UCC25640EVM-20. New transformer is wound to secondaty winding to 80V. Primary to secondary turns ratio is 2,36, Primaty bias yurns ratio is 11.
Calculation is attached…
Part Number: UCC25600-DESIGN-CALC Hello,
I am attempting to simulate an ac/dc design and would like to run a sim of the LLC / RC stage with these two parts however the models don't run in simetrix elements - please could I get uynencrypted models…
Part Number: UCC256404 Tool/software: Looking at technical articles:《LLC design considerations for audio amplifiers》, I found that there is a related article for APEC 2023,《 IS14.2 - Designing an LLC Resonant Converter for Audio Applications with High…
Part Number: UCC256404 Other Parts Discussed in Thread: UCC28019 , UCC24624 Tool/software: Dear Sir,
I have new issue with surge immunity for my charger for EV new design
the issue is when surge immunity test the POWER MOSFET for half bridge,POWER…
Part Number: UCC256404 I think that switching should not occur during burst OFF periods. However, under certain load conditions, switching at a high frequency of around 200 kHz is occurring during periods that appear to be burst OFF. Is this correct operation…
Part Number: UCC256404
Compared to UCC25630x datasheet, the document structure in SLUSD90E (UCC25640x, latest version) lacks a list of chapter/section entries between pages 40 and 66.
At page 39, System State Machine is presented, and then, the contents…