Other Parts Discussed in Thread: UCC27517A-Q1
Our customer consider to use UCC27517A-Q1.
Thei would like to know followimg data at VDD:9V and 15V.
RISE TIME vs TEMPERATURE (datasheetP8,Figure 12)
FALL TIME vs TEMPERATURE ( datasheetP8, Figure…
Other Parts Discussed in Thread: UCC27517A-Q1 Hi,
im going to use the gate Driver UCC27517A-Q1 in my design.
Unfortunately there is no value for the Minimum V IN_HYS Input signal Hysteresis.
I Need this for Performance calculation of the design…
Other Parts Discussed in Thread: UCC27517A-Q1 I have some question for Peak Current of UCC27517A-Q1.
Q1.
The absolute maximum of the datasheet includes "peak 4A at 0.5us" and a mention. (p3 Absolute maximumu ratings)
Is there any problem in the…
Hi,
External driver IC is available, such as
UCC27517A-Q1 Single-Channel High-Speed Low-Side Gate Driver with Negative Input Voltage Capability (with 4-A Peak Source and Sink) datasheet (Rev. B)
For high voltage startup circuit, you can refer to…
Part Number: SN74AHCT1G126-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 , CD40109B-Q1 Hi team,
I have a customer that wants to use the SN74AHCT1G126-Q1 for their design to move 3.3V logic to 6.5V, however the part says the max is 7.0V and they feel…
Part Number: SN74AHCT1G125-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 Hello,
I am using the buffer SN74AHCT1G125-Q1 for driving MOSFET with Vcc=5V. Gate resistance of 10 Ω was added, so gate current will be 500mA (5V/10Ω). Whether this buffer…
Hello Chase,
Thank you for the diagram, I see that the gate driver is being used as a low side driver which the UCC27211 can support, but confirm if the gate drive output will be driving a MOSFET referenced to ground only as shown in the diagram.
…
Hello Tamas,
I have reviewed the collateral available on ti.com for the UCC27517A-Q1 and it appears this data is not available for this IC.
I have attached below the available MTBF/FIT report and qual summary available for the UCC27517-Q1 available…
Part Number: TMS570LS1114 Other Parts Discussed in Thread: UCC27517A-Q1 Hi Team,
Our customer has this inquiry:
"We are using the Epwm4A and Epwm4B. Both Pins have the same purpose, so the connection to the pins is the same. We have not found any…
Part Number: CD40109B-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 Hi,
We have a requirement of level translation from 3.3V to 12V logic levels. Please let me know whether the part# CD40109B-Q1 is suitable for this purpose? If this can be used,…