Part Number: UCC27537
Hi team,
my customer use this on EV charging relay switch.
would you help check if this MOSFET is the right fit?
and check if the schematic has anything wrong?
Part Number: UCC27537 Other Parts Discussed in Thread: UCC27523 Hi team,
My customer is using UCC27537. The schematic is as below: VDD=12V, EN is floating and IN+ is from a opto-coupler.
We found that:
1. When we remove R6 and measure opto-coupler…
Part Number: UCC27537 Hi,
My customer is evaluating UCC27537 and have some concern about the Input signal threshold. From the table we can see the Vin_H(min) = 1.8 V and Vin_L(max)=1.2V. So in the worst case the input signal hysteresis is only about…
Part Number: UCC27537 Hi,
I would like to know if UCC27537 can use as a MOSFET driver for 12V turn on and off?
Like as below application for fan 12V control.
Part Number: UCC27537 This is my first time working with Altium and TI parts. I'm having trouble figuring out how to import the part into Altium and run a simulation on it. Any help of this topic would be appreciated.
Hello Lei,
I am a TI applications engineer who works with Jeff, and will work to help understand the concerns. At this point, it is not clear what is causing the behavior you are describing. I want to ask a couple of questions, and ask you to try a…
Hi,
I'm sorry if continuing this here is wrong, please inform me and delete this if it is.
I've tried to just turn on this MOSFET with 5V, but i only get ~3.5V at the LED which is not enough.
I'm planing to use UCC27537 to drive the MOSFET, will…
Part Number: UCC27537 Other Parts Discussed in Thread: UCC27533 Hi,
as below figure, when VDD is 7V, UCC27537 is till in off mode, but the IDD current is 300uA max current, what cause this high current?
in most case, UCC27537 is powered by auxiliary…
Part Number: UCC27537 The UCC2753x datasheet calls out the feature "Output Held Low When Inputs are Floating or During VDD UVLO". However, nowhere is the behavior specified. Ideally, the datasheet should provide a curve that shows sinking current vs.…