Part Number: UCC2808-1 Other Parts Discussed in Thread: TPS2811 , TPS2812 , LM5030 , Tool/software: Hello,
I'm looking for the LTspice files for the components UCC2808-1D and TPS2812D, it can be a .lib or .cir file. I'd like to simulate a DC/DC 'push-pull…
Part Number: UCC2808-1 Other Parts Discussed in Thread: LM5045 , UCC28951 Tool/software: Hi TIer
My customer would like to design an application with a 48VDC/50A input, converted to 2000VDC/1A, and then converted to 200VDC/5A after a long wire. In addition…
Part Number: UCC2808-1 Tool/software: hi team,
my customer need a solution as below:
Vin:18-36V Vo:24V Po=200W & 500W
i have recommend them to use UCC2808-1, do u have any other better solutions to recommend? thanks!
Part Number: UCC2808-1 Other Parts Discussed in Thread: UCC28083 , , LM5035 , UCC28250 Tool/software: Hello,
I want to design 12Vout, 20 A/30A solutions( Input voltage 24Vin) - isolated configuration.
I am planning to use TI Push Pull converters ex: UCC2808…
Part Number: UCC2808A-1 Other Parts Discussed in Thread: UCC2808-1 Can you comment on the following questions:
1) OUTA/OUTB Source Current: The UCC2808 lists -0.5A as a minimum whereas the UCC2808A lists -0.5A as a maximum. Is this an error? Should they…
Part Number: UCC2808-1 Other Parts Discussed in Thread: UCC2808A-1 , Do we have TINA SPICE Model for UCC2808-1 and UCC2808A-1? If not what is the nearest equivalent part available. I want to simulation Isolated DC DC Conveter Push Pull Topology 300KHz. …
Part Number: UCC2808-1 Hi, I have a question for pushpull IC UCC2808-1
I made 10Vin to 90Vout 1.5kW converter
the converter consist 800W two pushpull converters
they have common input and common output
I stabilize each converter to operate 800W output
…
Part Number: UCC2808-1 Other Parts Discussed in Thread: TL431 , LM311 , LM211 , LM211-Q1 Hi Experts,
I have two questions about how to use the UCC2808-1. First, please tell me about the duty ratio adjustment method (circuit). For example, what kind of circuit…
Part Number: UCC2808-1 Customer is using UCC2808 for isolated DC/DC 15Vin to +18V and -9V output with 5W-10W power in MD application.
Since layout area is constrain, customer would like to change the E-cap (220uF) to MLCC type, does it work?
Brian
Part Number: UCC2808A-1 Hi
I saw the typical application from datasheet of UCC2808AD-2,so can anyone help to explain below:
Q1: what is ① used for ?
Q2:why add an inductor connected to GND as noted with ② ?
thanks