Part Number: UCC28951 Tool/software: Dear Team,
Greetings!
I am Sonika from Applied Electro Magnetics Pvt. Ltd. We specialize in the design and manufacturing of advanced electronic systems for the railway, defense, aerospace, and industrial sectors…
Part Number: UCC28951 Tool/software: Hi,
Due to high power density, could we use differential amplifier to sense primary current in current mode of UCC28951/TMS320F28034PNT
instead of current transformer?
Thanks
Part Number: UCC28951 Tool/software: Hi All,
Thank you for all the help and support.
We are planning to use UCC28951 for our upcoming project 6.6kW ZVS Phase shift full bridge converter with the specifications of output voltage of 60V. But, the…
Part Number: UCC28951 Other Parts Discussed in Thread: UCC28950 Tool/software: I understand that UCC28951 is an enhanced version of UCC28950, but what is the difference?
Part Number: UCC28951 Tool/software: HI As per "e2e.ti.com/.../ucc28950-asymmetric-duty-cycle-operation" thread, it is suggested that in UCC28951 may not operate in very low duty cycle due to burst mode.
However in certain conditions, there are asymmetric…
Part Number: UCC28951 Other Parts Discussed in Thread: TIDA-01407 , UCC27282 Tool/software: HI,
Thanks for reply my previous noise issue related to un-balance duty cycle of OUTC & OUTD.
I follow the UCC28951 IC parameter of " TI Designs: TIDA…
Part Number: UCC28951 Other Parts Discussed in Thread: UCC28950 , UCC28750 Tool/software: Dear Team,
I am Sonika, a Hardware Design Engineer at Applied Electro Magnetics Pvt. Ltd.
We are currently using your IC, part number UCC28951. In the reference…
Part Number: UCC28951 Other Parts Discussed in Thread: UCC27282 Tool/software: Hi,
I am using UCC28951+UC27282, with Nosie issue at PWM output of UCC 28951, espically after PSFB turn on and loading current increase.
Another symptom is lower side…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Tool/software: Hello,
I am trying to design an isolated DC-DC converter with the following specifications:
Vin: 16-90 Vdc
Vout: 48 Vdc
Iout max: 30A
Using the TI Webench…
Part Number: UCC28951 Tool/software: Dear Sir,
We are using UCC28951 for designing PSFB Board for 4kW Charger. Can you give the procedure to do Fixed delay approach in UCC28951 for getting uniform DT. The dead time(DT) is Non-Uniform and there is…