Part Number: UCC28C52-Q1 Other Parts Discussed in Thread: UCC28C52 , UC3842 Tool/software: Hello,
Our customer is requesting a SIMPLIS model for the UCC28C52, or perhaps a very closely related device in the same family. Do we have a SIMPLIS model that…
Part Number: UCC28C52-Q1 Other Parts Discussed in Thread: UCC28C53-Q1 , UCC28C56EVM-066
Tool/software:
Hi Everyone
Can i use #UCC28C52-Q1 this flyback ic to design wide range input voltage flyback desing like 9VAC to 265VAC & output is 1.2 Watt…
Part Number: UCC28C52 Tool/software: I'm working with a WEBENCH-generated design for a flyback power supply, with the following specifications:
Input: AC 85 V - 265 V at 60.0 Hz
Output: Isolated 24 V at 2.5 A
WEBENCH specifies a TDK core and…
Part Number: UCC28C52-Q1 Hi, I wonder which design tool(s) is TI supporting/suggesting to simulate its ICs? free version of TINA does not have the component (UCC28C52-Q1) available in the library.
Thank you
Part Number: UCC28C52 Other Parts Discussed in Thread: UCC28C43 Hello,
I have an issue running a pspice simulation using the model provided on this site.
It seems the OLB file has the wrong pspice reference. When the OLB file is corrected, the simulation…
Part Number: UCC28C52 Hello,
I came across the UCC28C52 PWM controller IC and I wanted to know if it could be used in a SEPIC voltage regulator application. I can see from the datasheet that it can be used a s a Flyback converter but I am interested…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28C53 , UCC28C52 Tool/software: Could you pls help with calculation for soft start from the primary (controlling Cs Pin) and secondary (zenor diode and capacitor, slow vout rise)?
We r looking…
Part Number: UCC28C56EVM-066 Other Parts Discussed in Thread: UCC28C52 , Tool/software: I would like to know if there is any isolation regulator EVM available for the UCC28C52QDRQ1/UCC28C53QDRQ1 DC/DC controllers with flyback topology that uses an SSR…