Part Number: UCC28781-Q1 Other Parts Discussed in Thread: UCC28782 , UCC24612 , UCC28781 , UCC5304
Can a SR controller be used with this IC? I am thinking of UCC24612 since its suggested for UCC28782 in Webench design tool. Or is it a must to use an isolated…
Part Number: UCC28781 Other Parts Discussed in Thread: UCC28782 , , UCC5304 Hi,
I want to design a with following specifications:
Input voltage: 30V-200V (if too wide, can be made in two options, 30V - 90V, 80V - 200V)
Output voltage: 5V 6A
Currently,…
Part Number: UCC28781 Other Parts Discussed in Thread: ATL431 , TLV431 , , PMP22322 , , TL431 , UCC5304 , UCC28782 , UCC28C56H
Hello TI,
We have followed your EVM schematics and made a test board which does not start. The custom transformer is not made yet…
Part Number: AMC1301 Other Parts Discussed in Thread: UCC5304 , Hi Team,
When AMC1301DWVR sense feedback current ,Phase resistance is 0.25m Ω,we have some issue:
Test OPA output, find the Gate driver noise interference is serious, need help provide…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: UCC5304 , ISO7762 , , AMC1336 hi, I need to know if the below devices are in LOW voltage mode at the start.
UCC5304
ISO7762
ISO7742-Q1
thank you!
AC Guy,
The feedback I received from the UCC5304 team was the bootstrap-capacitor may have trouble charging or keeping charged at startup with a non-synchronous topology. Their recommendation is to use a synchronous configuration as shown in the UCC5304…