Part Number: VCA2615 My customer is considering to use the VCA2615. They would like to understand points to note when using in the 300 kHz frequency band of the VCA2615. In the data sheet, the lower frequency limit is cut at 500 kHz as shown in Figure11…
Part Number: VCA2615 Other Parts Discussed in Thread: LMH6401 Tool/software: Hi there, I am looking for a variable gain amplifier working in the range of 0 -12GHz. But after checking the VGA link ( https://www.ti.com/amplifier-circuit/pga-vga/products…
Part Number: VCA2615 Can you provide the ESD information for VCA2615 and the source of the data? A previous response to this question provided a table, Table 7.2 ESD Ratings, but the table alone does not provide proof that these numbers are for this particular…
Part Number: VCA2615 Hello all,
I use VCA2615 in ultrasonic application. On the page 18 of Data Sheet Table 5. shows codes for Feedback Resistor Settings.
I have come across that setting any code other than '1111' (Open) causes a significant increase…
Part Number: VCA2615 Hello mr. Chen Kung.
Excuse me for the late reply, I had no possible to do it.
I did not understand your answers.
>Please refer to the VCA2615 datasheet Figure 61 page 19, >Let's assume you are using active feedback termination…
Part Number: VCA2615 Hi Experts,
I am looking for the ESD sensitivity classification of VCA2615 as it is not included in the datasheet.
I am hoping you can help.
Regards,
Marvin
Part Number: VCA2615 Hi,
I have been observing that the linearity performance (Power Input vs. Gain/IM3) of the VCA2615 chip behaves different between different chip.
Some of them were way worse than the others in which, the gain curve was not flat…
My question was not fully answered. I added reply, indicating which part of my question was not answered, but so far 1 month I only got suggestion to close the thread.
Part Number: VCA2615 Other Parts Discussed in Thread: VCA2617 Team,
Could you please clarify the below? VCA261x are differential amplifers:
-VCA2617 specifies both the single ended and differential Maximum Input Voltage specification (see page 3 of…
Part Number: VCA2615 Hi,
I have two questions regarding VCA2615.
1 Maximum input voltage
Data sheet SBOS316D page 3, VCA2615 LNP Gain (G1, G2) = 00, maximum input voltage is 2.3 Vpp .
If there is a source signal Vs with a 100 Ohm series…