Part Number: VCA821 Tool/software: Hi team,
Does VCA821 have power sequence ? In the customer's use case, -5V comes to Negative supply(-Vcc) before positive supply ramp up to 5V. Is there any concern about that ?
Regards,
Morita
Part Number: VCA821 I design VCA821 for RF gian.
But I find VCA821 with temperature sensitive in this case,do you meet kind of problem before?
For detail,we power on the board with vca821(temperature at about 25°), after a while , temperature at about…
Part Number: VCA821 Other Parts Discussed in Thread: TINA-TI Hello I want to use VCA821 to design the input DC signal range in 0-1v or 0-2v Through the DAC input control chip pin Vg to achieve the output range of 0-3.3V, VCA chip power supply ± 5v Look…
Part Number: VCA821 Tool/software: Dear Specialists,
My customer is considering VCA821 and has a question.
I would be grateful if you could advise.
---
In the case of analog VGA, the output voltage may fluctuate greatly due to noise in the gain…
Part Number: VCA821 Hello Nick,
What is the exact gain formula of VGA820 with respect to control voltage. I have gone through the datasheet but couldn't get the problem formula with correlates gain with control voltage.
Could you please help me out…
Part Number: VCA821 Hi Team,
Is there any difference between the VCA821 on the EVM and the VCA821 on the official website? Do they all meet RoHS? Thanks.
Regards,
Charlie
Part Number: VCA821 Other Parts Discussed in Thread: LMH6518 , LMH6881
Hi team,
My customer is considering alternative device to VCA821 that can adjust the gain from the digital signal. I searched TI.com and found out LMH6518. But LMH6518's slew rate…
Part Number: VCA821 Other Parts Discussed in Thread: OPA820 , VCA820 , TINA-TI , OPA856
Hello Team, I am working with Automatic Gain controller on a high BW of 30MHz communication line.
For this application I have choose VCA821 VGA and OPA820 comparator…
Part Number: VCA821 Other Parts Discussed in Thread: THS3491 , VCA820 Hi team,
My customer want to use this device as below, Vs=+/-5V, Vppmax=2V, frequency=30MHz, AVmax=40dB, we use the datasheet's equation,
Rg>385 ohm, Rf<19.2k, so we use these two…
Part Number: VCA821 Hello team,
The D/S Table 2 specifies that RG = 18Ohm when G=40 (use case is AVMAX=32dB).
Figure 1 specifies that differential input voltage level should be close to 0.1Vpp when RG=18Ohm.
Is the input voltage level limited…