Part Number: VFC110
Hello
At long last, finally TI Stores does have this IC in stock.
We had gone around the proverbial mulberry bush locating this IC world over.
Now that both versions are available, VFC110 and VFC110AP , I am not able to
identify…
Hi Josh,
Josh Hollyer said: I want the duty cycle to always be 50% since I want to use this chip to clock an ADC,
The frequency is a function of input voltage and the VFC110 is not going to generate DC =50% response based on the internal topology. It…
Part Number: VFC110 Hello
We have some Signal Isolator using VFC110 with Fiber Optic Interface for shipment to France.
I can share the full Ckt if you want, but basically a TIA followed by V to F , transmission thru' FO
and on receiving end a F to…
Part Number: VFC110 SOS Reg availability of VFC110 or VFC110AP
I am very happy with the support from TI in the past
I am stuck and this may be considered an SOS.
In one of our Designs I've used VFC110 and I need to complete the Project.
Rochester…
Part Number: VFC110 Hello
In my last post I had mentioned that I was falling short of some 200 Nos
of VFC110 / VFC110AP / VFC110AP-2 for a Project of ours.
I have procured the rest from Rochester and some Distributors.
I have been offered some with a…
Part Number: VFC110 Hello
Mike was good enough to list out the Customer Support sites
regarding my issues of availability of VFC110AP.
Thanks to him and I have already written to two ID's
and waiting for their response.
Meanwhile , I have this supplementary…
Part Number: VFC110 Hello
I am happy with TI's support in the past on many occasions.
Earlier I had asked whether VFC 10AP was on EOL , to which
someone from TI assured it was not.
I've designed some boards with this and am falling short of some…
Part Number: VFC110
Hello
We would be requiring over 500 Nos of VFC110AP for a Project with long gestation.
I've two Q's:
1. Digi-Key Site shows Rochester Electronics VFC110AP-2, while TI's P/N is VFC110AP
Are both of them identical? Is…
Hsin-Che,
Typically, the maximum frequency of a VFC is not adjustable in monolithic Voltage-to-Frequency converters. The VFC32 allows for a much wider frequency range. Can you use this device? I do see also VFC320 and VFC110 for voltage to frequency operation…
Part Number: VFC110 Hello,
We are using VFC110 since 2012. All the batches we received until now are working fine. But we are facing problem in the last batch that we received in October 2020. As, they aren't behaving as they should.
Batch working…