Part Number: VIALUX-3P-ALP-4 Other Parts Discussed in Thread: ALP , DLPC410 This is right:
The original DMD in the system broke and a DLP7000BFLP was purchased to replace it.
That DMD is not recognized. I believe the ALP will default to 1080p.
…
Part Number: VIALUX-3P-ALP-4 Other Parts Discussed in Thread: ALP , DLPC410 I have a problema with my DMD vialux v7001. A piece of the DMD broke.
Part DLP7000BFLP was purchased and installed in the DMD.
But the DMD doesn't work. We had carried out…
Part Number: TUSB522PEVM Hi Team,
I have ordered the TUSB522PEVM and connected it between my Lattice Versa FPGA board and the Host PC. However, when I check USB Tree Viewer, the device is enumerated only as High Speed(USB2.0) instead of Super Speed…
Part Number: BYTES-3P-BE-AM6254 Tool/software: Dear TI colleagues
Regarding AM6254 SOC DDR interface, as the TI EVM design file shows the DDR4 is MT40A1G16KD-062EIT:E, I checked this components spec, the DDR4 speed ratio is 3200 MT/s, but the SOC support…
Part Number: J722SXH01EVM Other Parts Discussed in Thread: AM67 Tool/software: Hi,
I'm wanting to test flashing an image using super speed in u-boot on AM67.
All of the code is written as if it should support usb 3.0, but the device is automatically…
Part Number: TUSB8020B Hi,
If user does not use USB3 Super Speed on TUSB8020B, are "related pins" open? Such as U SB_SSTXP /M _UP /DNx, USB_SSRXP/M_UP/DNx. Please let us know.
Thanks and best regards, M.HATTORI.
Part Number: AM5728 I want to simulate SuperSpeed using the IBIS model on the AM5728. Which ModelSelector should I use for SuperSpeed for the target pin?
AC11 USB_TXN0 Selector_3 0.16771 2.41602E-09 4.75415E-13 AD11 USB_TXP0 Selector_6 0.173562 2.8275E…
Part Number: AM5728 I would like to simulate the following signals of USB3.0-SuperSpeed. Is it possible with the IBIS Model published on the Web?
If you can't simulate the SuperSpeed band with the published model, how do you plan to simulate it? (Are…
Part Number: TUSB9261 Other Parts Discussed in Thread: AM5K2E04 , , , Hello to everybody,
We have a boot issue during the mount of a Mass Storage on Sata interface, through the TI USB to Sata bridge.
For some random boot sequences, SSD mount is sometime…
Part Number: TDA4VM Hello,
Originally tested in SDK8.2 and recently with the latest SDK, USB-C is not stable in SuperSpeed mode. Issue is visible on both platforms J721-SK and J721-EVM. Test data is shared below from several combinations of cables and…