We provide a FreeRTOS implementation in the latest versions of C2000Ware. Look for it in the kernel folder.
I believe WHIS also provides SAFERTOS and OPENRTOS for C2000 devices: https://www.highintegritysystems.com/partners/texas-instruments/
Whitney …
Thanks Ralph, that really clarifies things. I think and addition to the TM4C like you said would be very helpful.
I will leave a note here for others that may peruse this post that I was able to use Stateviewer's OpenRTOS Viewer plug-in tool with FreeRTOS…
JohnS said: High Integrity Systems had a StateViewer Eclipse plug-in. www.highintegritysystems.com/.../ However I was never able to get that to work in CCS. It is possible that it assumes that gdb is being used as the debugger. I have had a look at StateViewer…
Part Number: AWRL6432 IWRL6432 AWRL1432 IWRL1432 Other Parts Discussed in Thread: IWRL6432 , IWRL6432BOOST
xWRL6432 and xWRL1432 are ready for evaluation!
Product folder and EVM:
IWRL6432 Product Folder
IWRL6432BOOST EVM
AWRL6432 Product Folder
AWRL6432BOOST…
VGA_out.y.txt customImage640x480.raw.txt VGA.y.txt customImage_output640x480.raw.txt Hi Champs,
I am using CCS 5,4 for EVE simulator. its getting compiled and i tried to run the morphology testcase, it worked fine.
Now i wanted to check with edge detection…
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file : (convert…
Hi Praveen,
I referred the section 3.6.5, optimized frozen graphs for MobileNet and tried to run the generated .pb but it's also showing error in tidl_log.txt file as :
"
TF Model File : ..\..\test\testvecs\config\tensorflow_models\mobilenet…
Hi,
I mean I can play it in VLC, but it play not smoothly. when I use the Elecard StreamEye Tools to play it , it is smoothly, i
I have uploaded the video . Because i want to upload the video ,so i have to change the file`s expanded-name to txt, it is not…
Hi Louis,
It looks like one of the redistributables is not installing correctly on your machine. Can you please:
Save the attached file as .exe
Double click on it to run it.
Follow the prompts and report any errors.
If no errors, please delete the contents…