Part Number: WL1835MOD I'm trying to install wl18xx driver for Debian jessie, my board is ACME RoadRunner.
I'm following the instruction in the following guide: http://processors.wiki.ti.com/index.php/WL18xx_System_Build_Scripts
dso_dlfcn.c:(…
Hi Ivaylo ,
I followed the steps you suggested but the result is same.
Android comes up on the Blaze display but it freezes i.e i cannot access anything. In the debug console the kernel gets stuck at this point ' [ 15.202484] omapdss DISPC error:…
Hi Madhu,
I am currently unable to continue with the work due to lockdown in our locality. I shall inform if there are any further developments.
You must ensure that your device is configured in SCI-A serial bootload mode. Please refer Boot ROM…
I have a simple UART echo working with UART1 on the launchpad using Pin16 and 17. I've attached my .out (remove the.txt extension). You can load and run this using CCS. Since Pins 16 and 17 are JTAG pins TDO and TDI you'll have to use SWD (2-wire JTAG…
I just ended up changing the .out extension to .txt. Copy and pasting it as text just pastes **ELF** without getting all of the random characters.
uartecho_MSP_EXP430FR5994_TI.txt
Hi Venkat,
I've attached my "audioSample.out" app from the following application.
Also, attach your binary so that I will try at my end.
C:\ti\pspdrivers_01_30_00_06\packages\ti\pspiom\examples\evm6747\audio\bin\iDebug
audioSample.txt
Hi Jai,
Some status update:
With the SAME sensor driver (One-stream-Only currently), I used gst-launch-1.0 and v4l2-ctl to capure some frames, It looks gst-launch-1.0 (I tried to remove 'io-mode=dmabuff' keyword from the command line, but it still…