Other Parts Discussed in Thread: XIO2001 , XIO2000A Dear Sir
I want to realize XIO2000A could support ASPM function or not. Because XIO2000 and XIO2001 Errata shows that these two parts do not not recommended to use ASPM function.
Thank you.
Other Parts Discussed in Thread: XIO2000A Hello,
We are using the XIO2000a PCIe to PCI Bridge for many years.
Now we discovered that when the XIO2000a receives a message Set_Slot_Power_limit of 0 Watt it starts sending PM_PME messages to the root complex…
Other Parts Discussed in Thread: XIO2000A Greetings,
I recently bought a StarTech PCI Express to PCI breakout box which uses the xio2000a chip. My application requires more power than is supplied with the given configuration, they stepdown 12V, 3A, and…
Other Parts Discussed in Thread: XIO2000A , XIO2001 Dear Community:
I need to access Memory-Mapped TI Proprietary Register Space of XIO2000A. How do I find the base address where those registers are mapped to?
lspci -vvv gives me:
PCI Device behind…
Other Parts Discussed in Thread: XIO2001 , XIO2000A AudioScience makes PCI and PCIe plugin audio adapters for PCs. See < www.audioscience.com >. We have done
many PCI designs + drivers and more recently PCIe designs based on the XIO2000A and XIO2001…
Other Parts Discussed in Thread: XIO2000A , XIO2001
We have 2 designs that use a C6205 to perform PCI bus mastering operations. They are as follows
1) PCIe bus <->XIO2000A <-> C6205
2) PCI bus <-> C6205
In both cases the C6205 is…
Loic,
There are no platforms on the market that we are aware of on which the XIO2000A does not function.
There was a spate of Intel H55s that came out with problems, but after a BIOS update from Intel, all the problems were gone. We have no insight…
Other Parts Discussed in Thread: XIO2000A
Hi TI-Group...
Did anyone of you use any TI DSP such as DM648 or DC642 in combination with a PCI-PCIe bridge such as XIO2000A?
We want to use DM648 on a PCI card and connect it through a XIO2000A to a 1x PCIe…
Part Number: TMS320C6674 Other Parts Discussed in Thread: XIO2000A Hi,
We are having C6674 based custom PCIe board. We are trying to use the device in Linux KVM/Qemu virtual machine. So on the host Linux machine, there are vfio kernel modules. When virtual…
Elias,
It's rather difficult because I am trying to coordinate with Startech who provide the equipment which hosts your chip to get answers to your questions. I do not yet know if the XIO2000A is configured with an external arbiter enabled. I believe…