Other Parts Discussed in Thread: AM3874 , XIO2000A Hi,
We use the DM814x/AM387x EVM Rev. D eval board (AM3874). Using the Using the Linux EZSDK 5.04 link training fails with some PCIe cards. One card is using a Marvell 88SB2211 PCI Express-to-PCI Bridge…
Hello Marko,
Knowing which device you are using is much better.
You can find the IBIS model for the XIO2000A in the below link.
Regards.
http://www.ti.com/product/xio2000a#simulationmodels
Hello Keith,
There is no released version of XIO2000A Errata.
However I am attaching an image that could be useful.
We encourage you to use the XIO2001 which is a more robust device and has fixed the erratas of the XIO2000A.
Don't hesitate in contact…
Hi Elias,
I see what happened, we have another similar board that also exhibits this behavior, and it uses the XIO2000A bridge device instead of the XIO2001. I mistakenly captured the dump for this board instead of the board with the XIO2001. I'll try…
Other Parts Discussed in Thread: XIO2000A , XIO2001 Can XIO2000A I (Industrial Grade) , support 66MHZ operation. I am refering to SCPS155C , April 2007 Revised October 2008
Pls kindly help to confirm because i intend to use XIO2000AIZZZ to replace XIO2000AZZZ…
Other Parts Discussed in Thread: XIO2001 , XIO2000A , XIO2001EVM Hi,
my customer plans to use XIO2001, but now they have production based on XIO2000. And the ask for errata for this device, which was removed from the WEB. Could you help somehow?
Isara, Srirami,
Is the usage of XIO2000A to connect to PCIe downstream device possible? Because in the scenario mentioned by Isara, the PCIe device will be an Endpoint.
Regarding U-Boot, the PCI host support for DM6467 in U-Boot is not available and…
Currently I'm unable to test 33MHz over the XIO. When EVM648 is jumpered to run at 33MHz inside the XIO2000A EVM, the PCs BIOS will not boot. Is there a configuration somewhere to force XIO to 33MHz? Or is it correct that XIO automatically detects 33…
Other Parts Discussed in Thread: XIO2001 , XIO2000A Hi,
maybe a very basic question...
I have a PCI device (XIO2001) connected to the DM648 PCI interface.
I think that the basic mechanism to communicate to a second PCI device is: move an "address window…
Other Parts Discussed in Thread: XIO2001
Hello,
we use the XIO2001 to build a PCIe card and connect the bridge to a PCI core. Using DMA we copy data from the card to the RAM of the PC. About 5 minutes after starting the operation, the PC freezes.…