Hi Matthew,
I have a few ideas what you could also check:
1. Remove D1.
2. Power the XTR110 by +24V, with removed D1.
3. Mount a 470nF cap directly to pin 12.
4. Take a transistor which is "smaller" than the MJE3055. Try the BD139 or similar…
Part Number: XTR110
Dear Technical Support Team,
My configuration of XTR110KU is following.
Vin: 0V~10V
Iout: 0mA~20mA
I adjust the offset pin(Volume register).Then almostdevice show 0mA(target is under 4.8μA) when Vin=0V after adjusting register…
Part Number: XTR110 Other Parts Discussed in Thread: LM324 Hi team,
I want to use XTR110 realize +/-200 mA AO circuit, I have seen a circuit in the DS fig.8. But I am clear about how VIN can control T2 on/off? Could you share me the principle? Thank…
Part Number: XTR110 I've wired up the Basic Circuit Connection in Figure 1 (page 6) of the XTR110 data sheet.
Supply voltage is +24 volts (between pins 16 and 2). Also ran the circuit with 12v, as 24v pumps too much wattage through my load resistor…
Thank you so much for your detailed response. Just one additional question, what do I have to do to receive updates on product availability? Is it enough to click the 'alert me' button on XTR110 family website?
Best regards,
Agustín Méndez
Part Number: XTR110 Hello, All,
At datasheet, page2, i see operation temperature for XTR110KP as 0 +70C. At page12 operation temperature has shown as -40+85C. Please advise correct operation temp range for XTR110KP
Best regards,
Dmitry
Part Number: XTR110 Other Parts Discussed in Thread: OPA191 The data sheet for XTR110 has a FIGURE 10. 0A to 10A Output Voltage-to-Current Converter.
1) Shouldn't pin 10 be to Com? That pin is not shown. 2) if I want my input to be 0 to +5V, Pin 10…
Hello Jose,
The offset trim circuit in the XTR110 is not meant to provide volts of offset to account for input signals that do not have a zero-scale level of 0V. The offset trim circuit is designed to correct for around 100mV of offset due to circuit…
Other Parts Discussed in Thread: XTR110 , XTR111 Hi all,
After using XTR110 for a new design we have some questions about it:
We need an operating temperature range of -40-85ºC so we chose the ceramc AG version. Now this model is NRND and it is…
Other Parts Discussed in Thread: XTR110 Hello.
The customer wants to use it as VI converter of the output (0-40mA) for input (0-10V). And the customer is going to use XTR110. Expand SPAN by connecting resistance between 1 -16 pin pins in parallel with…