Hello Luis, Thank you for your reply. The user guide of the XTR111 recommends using a bipolar TVS diode (MPN - SMAJ40CA ). The same output terminal act as the analog voltage/analog current output. So for 4-20mA output, the voltage can be more than 10V but…
Part Number: XTR111 Other Parts Discussed in Thread: LM358 , TLV2170 , TLV9302 , OPA2170 , LM7705 , TINA-TI hello. I've been trying to get 4-20ma output with xtr111 for a while. I'm applying the output of lm358, which has a gain of 10, giving 0-10v output…
Part Number: XTR111 Hello team,
I received questions from the customer.
Adding the recommended external current-limiting circuit shown in the datasheet, as shown in the following figure, will prevent a current flow of more than 50 mA even if the load…
Hi Daria,
As you have mentioned, the device operating range is from -40C to +125C, where datasheet typical span error over the temperature range is approximately ±0.1%. However, the XTR111 electrical characteristics table only offers assurances for…
Part Number: XTR111 Hello Team, I am planning to use XTR111AIDRCT for one of our products to get a 4-20mA output current corresponding to a sensor output. The 4-20mA output current will be fed to a connector. A 0-10V analog output voltage shall be provided…
Part Number: XTR111 Hello,
I´m using XTR111 with MOSFET TP2510.
Now it´s immpossible to find it.
I´m searching another MOSFET to replace it.
BSP170P and NTF2955 are without stock.
Do you know another MOSFET to replace TP2510?
Thanks…
Part Number: XTR111
Hi,
We dont want to use externally adjustable voltage regulator of XTR111. is it correct to connect REGF and REGS by 2.2nF capacitor as shown in below image?
Please let me now my understanding is correct or not.
Regards,
Nikhi…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111
circuit requirements that ı need
VSP:16-40V input voltage range 0-5V output current range 0-20mA Output maximum load resistance: 600ohm
SI3459BDV-T1-GE3
( https://www.digikey.com/en/products…
Part Number: XTR111 Hi Sir,
We are using the attached design for generating the 0-20mA from 0-5V input with Vsp-12V.
We got the results as per the calculation Iout-10*(Vin/Rset). For 0V- 0mA & 5V-20mA
But after 2 or 3 iterations the results are ch…
Part Number: XTR111
Hello, the output end needs to be protected against reverse connection when connected to 24V power supply. A diode D01, 1N4148, is connected in series in the channel. Is this connection feasible and has any effect on current output…