Part Number: XTR305 Other Parts Discussed in Thread: XTR300 , TIPD155 , DAC8563 Hi team,
Our customer use XTR305 in such a system, XTR305 input is an DAC signal. When customer OD pin is low, if DAC has a output, the XTR305 has a small output at the…
Part Number: XTR305 Other Parts Discussed in Thread: LMV324 , LM324 , The circuit below has been powered with Vin = 24V and Ax connected to Power supply 0V via a DVM in current measurement mode. Accidentaly the GND connection of the circuit has been left…
Part Number: XTR305 Other Parts Discussed in Thread: XTR300 Hello! I have some questions about thermal problems on my pcb. I designed a PCB for 0-10V / 0-20mA Output. It's was driven by ESP32. With my software I can switch from 0-20mA to 0-10V output…
Part Number: XTR305 Other Parts Discussed in Thread: LM317 I use 3 XTR305s in my design and output 0~5V or 4~20mA. The negative power supply of the XTR305 is designed to supply -9V. The TC7662 is used to provide -9V, and the output current of the TC7662…
Part Number: XTR305 Other Parts Discussed in Thread: XTR300 , XTR117 , XTR111 , XTR115 , XTR116 Hello guys,
One of my customers is using XTR305 for their current products. They are going to start developping next product soon.
One of the next product…
Part Number: XTR305 Other Parts Discussed in Thread: XTR300EVM , XTR300 Hello,
I've this circuit of XTR305 for Analog Output. Even if the output for DAC which is input to XTR305 is there, still XTR not giving output.
Below is the circuit I've prepared…
HI Kaileh,
The XTR305 requires bipolar supply; it requires a minimum negative supply of V(-)=-5V.
The device can operate with assymetrical voltage supplies, for example, V(-)= -5V and V(+) = +24V.
However, the device will not operate properly with…
Part Number: XTR305 Other Parts Discussed in Thread: XTR300 Dear TI Team
I would like to know about the Voltage Mode Nonlinearity Distribution of TXR305.
If you check the Voltage Mode Nonlinearity Distribution of XTR305, it will be as shown in the…