Hi Matteo,
Can you please share the XTR305 complete schematic?
Is the XTR305 output desired +/-10V from a 0.4V to 2.9V input signal at the XTR305 input?
Is the microcontroller PWM 3.3V in amplitude or 3V?
Thank you and Regards,
Luis
Other Parts Discussed in Thread: XTR305 Dear Team
XTR305 : output Voltage range 0 to 10 V is not coming, current 0 to 20 mA is working properly
PFA schematic, request you to provide your feedback and solution.
Thanks,
Chetan
Part Number: XTR305 Other Parts Discussed in Thread: XTR111 , OPA192 , INA592 Dear TI Masters,
XT305 and some other ICs are able to deliver an output current from 0 to 24mA, but I'm in need of some 4mA more. It means an output current form 0 to 28mA…
Hi Jan, Hi Raymond,
I tend to agree with Jan. As the XTR305 is a chopping device I feel uncomfortable when totally omitting C5. So, I would recommend the following compromise:
jan_xtr305.TSC
Kai
Part Number: XTR305 Other Parts Discussed in Thread: XTR105 XTR305 has been configured as per figure 40 of the datasheet with V+ at +24V, V- at -5V and logic supply at +3.3V. M1 tied to DGND with M2 and OD\ being controlled by a PIC microcontroller. Ciruit…
Part Number: XTR305 Hi,
XTR305 has voltage output mode and current output mode.
Is to switch these mode assumed during working?
Best Regards,
Kuramochi
Part Number: XTR305 Hi,
I recognize that XTR305 has output current limit function.
However, it is recommended to add external protection on the datasheet, "8.2.2.10 Output Protection".
I think that external protection is not necessary if internal…
Part Number: XTR305 Hi,
I have a question about Figure 46. on the datasheet.
It is described that "external protection diodes may be necessary to handle excessive currents" on the datasheet.
Does "external protection diodes" mean above diodes…
Part Number: XTR305 Other Parts Discussed in Thread: TINA-TI Dear Sir or Madam,
I have a problem with the simulation of my XTR305 circuit in LTSPICE simulator.
I downloaded the simulation file XTR305.txt from your website and inserted it into LTSPICE…