Hi,
I guess you were sharing your header file in your last reply, right? I copied your code in my test project in CCS v9.0.0 and it showed similar error with yours.
It seems there is unresolved symbol which referenced in the rts430x_lc_sd_eabi.lib…
Hello Li,
There are several code examples for the CC430F5137 here: http://dev.ti.com/tirex/explore/node?node=AL8AXAmsHxTrOvvkPOcfwQ__IOGqZri__LATEST
The UCS module is what controls the clock frequency, so I would look through those examples to see…
Part Number: CC430F5137 Other Parts Discussed in Thread: UNIFLASH Hi,
They have a problem that Only segment D (00187Fh to 001800h) on Information memory (flash) has occurred to ALL_F. Both of Segment C 0018FFh to 001880h and Segment B 00197 Fh to…
Part Number: CC430F5137 Other Parts Discussed in Thread: MSP-FET hi,
a customer of mine took an MSP-FET adapter and CC430F5137 device, as he wants to do a kind of RF tag device running with 433Mhz.
He got the slac525b.zip file too and is using SmartRF…
Part Number: CC430F5137 Other Parts Discussed in Thread: CC1101
I am wondering how exactly this built in address check is working.
It should be enabled but I still get messages not intended for me.
0x86, // PKTCTRL1 => Address check and 0 (0x00…
Part Number: CC430F5137 Dear TI Team,
In the datasheet, from page 71 to 83, TI have provided detailed RF data for frequencies, 315, 433, 868 and 915MHz.
Currently, we are designing for 779 to 787MHz, which the chip can support; but will TI be able…
Hi,
Thank you very much.Initial assignment was to include location coordinates of at least 30 locations.Hence to shorten the code length I felt a dedicated storage would be better.
I will incorporate your logic for 15 locations and try the output…