OK. I use sdk 10.0 with native linux driver. For our custom board, I disabled port 1 and port 2 of cpsw5g.
and the linux booting log like:
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.6.32-g6de6e418c80e…
Hi Umesh,
Couple comments:
Do you need to support EtherCAT slave? If so, you will need to order the "E" or "F" version. (see attached)
The Ethernet MACs supoprt MII, RMII, and RGMII - They do not support SGMI
I would start by evaluating the…
Hello Jianzhong
Thank for your guideline.
We found /dev/video0,1,2,3 and /media0 device files.
May you provide additional guidiline how to view the camera streams? and 4 camera streams saperately. Thanks.
Our DTS setting:
video_decoder_mipi…
Hi Karan,
Thanks for your reply.
Karan Saxena said: Do you have a valid file system?
Yes, the customer has valid system, just on NFS, and the file system is obtained by the boot parameter. The parameters are as follows:
setenv bootargs console…
Hello,
Those are inserted as images sorry about that. Those are just me attempting to upload the PortabilityLayer.dll throught labviews "import wizard library" and having no success because we receive the following errors:
Import Shared Library…
Thanks for the schematics Bart,
The GUI metering results page is completely blank, white. If I click on comms #2, results page appears with fields show and no data. The comms button remains grey.
For safety, I've pulled the short at J9 on the power…
Part Number: BQ20Z655
Hi, Sir:
I tested the bq20Z655 for 2s application.
After ox46 to turn on the CHG & DSG mosfet. I can measure the Pack output voltage.
I charged the pack, charging is OK.
After charged, the dsg turn off, so pack output voltage…
Part Number: TDA4VM HI, TI expert
We using SDK 07_03_00_07 and run Linux kernel, when run our own surround view app that can get some errors when lead system hang, the log as follows, please help me fix this problem, thanks!
2022-09-21 14:06:59…