Part Number: WL1835MOD Tool/software: Linux First, I believe it would be helpful for me to explain what we intend to use the BBGW for in our Capstone project.
The goal of our project is to relay (extend) the live stream video data from the DJI Phantom…
Yimin,
Here is a patch that I have applied to our Linux kernel to address this issue. It is for linux-processor-sdk-3.14. It requires that all SPI chip-selects on a SPI bus must all be active-low polarity.
I hope that it also works for you.
…
Part Number: AM3358 Hello team,
I have designed a custom board of AM3358 and using SDK ti-processor-sdk-linux-am335x-evm-06.03.00.106.
I was able to use the GPIOs of banks GPIO0,GOIO1,GPIO2 in the user space using /sys/class/gpio export .
But, the…
In this forum we only support the Linaro ARM gcc compiler which ships with Code Composer Studio. I have it installed on my Windows laptop. When I look at the version I see yet different information ...
C:\dir>C:\ti\ccsv6\tools\compiler\gcc-arm-none…
Part Number: MSP432P401R Tool/software: Code Composer Studio Apologies in advance for this being sort of a multi-topic question but I think all the steps relate to each other.
Currently we are using a MSP432 Launchpad board as a daughterboard on our…
Part Number: SK-TDA4VM Tool/software:
Hello,
I have been working on TI SK-TDA4VM Board for which I have built the v9.1 Image using below config file.
./oe-layertool-setup.sh -f configs/processor-sdk-analytics/processor-sdk-analytics-09.01.00-config…
Part Number: DM8107 1. 8107 add snapshot
如下图,在enc link里面添加了一路mjpeg的编码,修改如下;
As shown in the figure below, a MJPEG encoding is added in the ENC link, which is modified as follows:;
There was only one H264 encoding
Via Venc_ Getbitstreambuffer…
Other Parts Discussed in Thread: DM3730 hello :
as we known the dm3730 have 1. IVA2.2 subsystem with a C64x+ digital signal processor (DSP) core 2. SGX subsystem for 2D and 3D graphics acceleration to support display and gaming effects;
could any…
Part Number: AM4378
Tool/software: Linux
Dear Experts,
I have 4 questions listed below I'm hoping somebody can help me with.
I'm using an AM437x GP EVM running ti-processor-sdk-linux-am437x-evm-03.02.00.05 pre-built image booting from SD card…
Lisandro,
Thanks for the background and let me try to address your specific questions:
user4667683 said: - Is Uniflash 3.4.1 the more appropriate tool to flash Sitara AM335x based boards via USB (or Ethernet)? Or is there any other better tool?
…