Part Number: LM25118
Tool/software: WEBENCH® Design Tools
Dear team,
I'm try to setup a LM25118 power stage to supply a embedded board 5V@4A maximum, input voltage is between 3.0V and 12V.
After calculation and exporting from WEBENCH I can see…
Hi Praveen,
In the design calculator that you have shared cell No. F62 has been tampered because of which the the 'Maximum steady state FET Junction Temperature (TJ,DC)' , 'SOA margin during "hot-short" or "start-into short"' calculations have gone…
Mike,
It is not recommended that LVDS is used for a multi-drop scheme as these devices are designed for point-to-point applications. For a multi-drop scheme, I would suggest using M-LVDS or LVDM devices. He is a guide with some useful information about…
Other Parts Discussed in Thread: TPS40170 I'm working on a switching supply using the TPS40170 that has the following parameters:
Input: 5.8 to 31V
Output: 5V 5A
I've mostly used Webench to generate the design. It works very well with a 12V input…
Other Parts Discussed in Thread: MSP430G2553 #include"msp430g2553.h" void configTA0(); void configTA1(); unsigned int i =1,count=0,j=0,k,j_prev=0; // used as counters unsigned int c1,c2,cc,dump; char anand = 0x01; // count for capacitance measure //-…
Hello,
Playing around with the TRF7960EVM, I hooked up my scope and set the following under the TFF7960 EVM control application under Test t ab using Firmware Revision 06_16_2011 (programmed LED5 to have trigger out)
0x10 Write single register …
Other Parts Discussed in Thread: TPSM82480 Hello,
My customer is looking for an alternative to Murata MPDY301S (please refer to the attached datasheet below) that would be EOLed soon.
Any recommended TI solutions? murata_ty41_sea-1186439.pdf
Best…
Kai,
Roughly it is b'n rx antennas for far object.
Is your object near and are you trying to apply near field correction as mentioned in the attached guide?
Thanks
Yogesh
user_guide.pdf
Is the described fault injection method only used on a limited case for this test?
No, whatever is done remains part of the design as the entire design is analyzed for Intrinsic Safety compliance and is frozen after certification is granted.
Then…