Other Parts Discussed in Thread: LM5155, LM5157
Tool/software:
How can I use an LM5000 in a fully galvanically isolated configuration? The datasheet application diagram for a flyback converter uses a shared ground for the input and…
Hello Brigitte
Thank you for the exact answering. Then it is as I expected and got it verified with you.
One last thing now. Then I can resolve my issue.
Regarding the statement "If your input supply is limited, this limits your output power and…
Hello Tommy,
I have not seen an update from you for nearly two weeks,
Did you manage to pass the test?
Was it enough to change some components or will you need to add a filter?
Thanks and regards,
Harry
Hi Rizwan,
I have not seen an update for the last x days, so I assume the questions are answered.
I close this thread now. If there is still something open reply and the thread will get open again.
If you have any other question or of the thread gets locked…
Hi Alex,
I have not seen an update for the last 24 days, so I assume the questions are answered.
I close this thread now. If there is still something open reply and the thread will get open again.
If you have any other question or of the thread gets locked…
Hi,
I'm planning to use the LM5000 to generate 48v from a 16v source.
The Webench calculator gives me different values than the Datasheet's schematic.
Which schematic do you recommend? (image in attachment)
Thanks
Hi Experts,
The reference design of LM5000, that the inductance is large different between Webench and datasheet.
Please refer to the below schematic.
May I know the reason of difference?
Generally, which one is the better design…
Hi everyone!
I'm designing a boost converter with the LM5000, but I'm facing some troubleshootings.
Firts, some informations about the circuit:
- I designed the circuit using WEBENCH;
- The input varies between 18V and 30V…
Hi
Can I see the bode plot of the LM5000 circuit?
It seems not to show it on WEBENCH.
I would like to adjust phase compensation components with not only loop frequency but bode plot.
Conditions are followings;
VIN=10V~14V, VOUT~48V…