Tool/software:
I would like to know the low frequency cutoff of the LMH6401IRMZ.
Tool/software:
I would like to know the low frequency cutoff of the LMH6401IRMZ.
Hi Team,
I would like to address the LMH6401 SPI via opto coupler
The operating frequency is 10KHz
I saw that the LMH6401 specifies only maximum frequency. Is there any minimum frequency limitation?
Best regards.
I am referring to the old post --> LMH6401: Need DC offset drift information
Can I request for the DC offset drift information and data as well?
I will be using the LMH6401 for DC-coupled application.
Thank you,
Regards,
Sek…
The following files contain S-Parameters for the LMH6401 at three gain settings (Max gain, 10dB, and -6 dB).
LMH6401_MaxGain_Vs=5V.s4pLMH6401_Gain_10dB_Vs=5V.s4pLMH6401_Gain_-6dB_Vs=5V.s4p
Hi Team
i am using the PSPICE model of LMH6401 and simulating it in LTSPICE
What are the B0 - B5 ports? How do i connect them?
How can i choose the gain?
Please help in advance
Regards,
Roey
Hi,
Is it possible do daisy chain 32~64 of these in the same SPI bus. The Sclk and SDI is tied. What is the current for these pins?
Thanks,
Vicky
Hi,
I would like to daisy chain 64 of thes parts on the same SPI bus direct tie the SCLK and SDI pin together with separate independent CS and SDO. Is it possible? Can you tell me the…
Hello E2E Experts,
I'm not sure if this is the best place to report this bug but the PSpice TI Component Library database has an issue with the LMH6401 Model Test Circuit. It refers to…