Other Parts Discussed in Thread: TMS320DM6446,
Hi Support Team.
In the Qualification Summary, the results of ESD-HBM and CDM are described as "See data sheet".
However, the datasheet does not show the results of ESD…
Hi Support Team.
In the Qualification Summary, the results of ESD-HBM and CDM are described as "See data sheet".
However, the datasheet does not show the results of ESD…
Hello Team,
We are trying to a signal simulation on the DDR2 Memory Controller, but the IBIS model published on the product page does not appear to have the DDR data bus registered.
Could you provide IBIS model that can be used…
Hello,
I have the following issue on kernel 3.14
GPIO7 is interrupt number 71 on the DSP CPU, and 55 on the ARM CPU.
Using the rather dated methodology of requesting an IORESOURCE_IRQ for IRQ 71 allows the interrupt to work…
Hi,
An undershoot (-0.8 V) of the following short time (20 ns) has occurred with the DM6443 and flash connection.
Undershoot is not specified in the DM6443 datasheet.
Is it acceptable range?
Please tell me the allowable undershoot…
Hi team,
SoC (TMS320DM6443) has three onboard timers of which two are foreseen for usage by both ARM and DSP.
However in some cases DSP cannot access it.
In concrete case upon booting,
ARM runs first by only pre…
Hi,
I am new to ccstudio im using tms320dm6443 davinci processor kindly anyone can tell how to download my program into the processor is there
any separate tool available for downloadin or we…
I understand your confusion. But you are not using the -mv option as intended. The -mv option is intended for naming the CPU core. A TMS320DM6443 contains two CPU cores: a TMS320C64x+ DSP core and an ARM926EJ-S MPU core. So, when you are building code for…
Hi there
What is the suggested way to link a clean DSPBIOS 6 project (i.e. no use of DSPBIOS 5 compatibility layer) with dsplink?
dsplink uses DSPBIOS 5 API calls (even when built for DSPBIOS…
hi all
the platform i'm working on is a TMS320DM6443. timer 1 is owned by our application running on the ARM, so timer 0 is available to the DSP.
from the DSP/BIOS 5 documentation i gather that the CLK…