Other Parts Discussed in Thread: TMS320DM6443
hi all
the platform i'm working on is a TMS320DM6443. timer 1 is owned by our application running on the ARM, so timer 0 is available to the DSP.
from the DSP/BIOS 5 documentation i gather that the CLK module uses TIM12. because timer0:TIM12 is the only timer that can be run off an external clock i would like to use timer0:TIM12 for my application and have DSP/BIOS use timer0:TIM34 to drive the CLK module. is this possible at all?
i also tried to tell DSP/BIOS to leave the timers alone using
bios.CLK.ENABLECLK = false;
so that i can have my custom timer settings and interrupts, but this gives me a Can't modify read-only field error on that very line of the tcf script.
these are the versions i use:
bios 5.32.04
cgt 6.1.13
cheers,
sam