Hi Vinu,
I format mmcblk0p1 as ext4 partition and redo the work. Run your command as following:
Fullscreen
20260602_1655_test_SPL_falcon_eMMC.txt
Download
s writtenrst 512 bytes of eMMC boot0 to verify tiboot3.bin was
root@am62pxx…
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: MMWCAS-RF-EVM , AWR2243
Tool/software:
Hi expert:
I'm using the MMWCAS-RF-EVM along with the MMWCAS-DSP-EVM to collect data using mmWave Studio 3.0.0.14. The RF-EVM has AWR2243 radars…
Part Number: DRV8334EVM Other Parts Discussed in Thread: DRV8334 Hello TI Support Team,
We are using the DRV8334 EVM to drive a 24 V Ametek BLDC blower motor with 6-step trapezoidal commutation , controlled entirely via MCU-generated P WM signals. No…
Part Number: TMDS181 Other Parts Discussed in Thread: TCA9517 Tool/software:
Tool/software:
Hi team,
There is an "DDC read failed" when TMDS181 at SRC configuration. From customer schematic, this circuit can be configured as SNK side and SRC side…
Part Number: AM625 Hi,
I’m working on AM625 SK EVM using TI Processor SDK Linux RT (09.02.01.09) . I have:
LVDS panel with timing:
clock-frequency = 65000000;
hactive = 1024;
vactive = 768
hfront-porch = 24;
hback-porch = 160; …
Hi Fabian,
Fabian said: But when plugging in a USB device, it's not mounted at all.
Is the USB device getting recognized?
Can you try connecting any other USB device , and see if it is detected?
I tried testing the same on my end on TI J7200 EVM…
Hi Frank,
What is the logic level of you SPI? What do you have VIO and VDD connected to on the EVM? Maybe a picture of your entire EVM configuration would be helpful so I understand your setup.
This should not be the behavior, though I see what you…
Hi Vinu,
I implemented the suggested change by moving both regulator nodes out of &exp1 and placing them as siblings of vmain_pd , vcc_5v0 and vdd_mmc1 under the root ( / ) node. I rebuilt the DTB, updated the board and collected the requested regulator…