Part Number: ADS5401 Other Parts Discussed in Thread: TMP75 Hi team,
Could you tell me how to convert a binary to abs decimal date on temp sensor register?
If there are any equations for the conversion, please let know where it is in datasheet.…
Part Number: ADS5401 I'd like to inquire about the ADS5401's maximum output sample value expected. With the data format set to two's complement, I'd expect the possible integers represented to be from -2^(N-1) to 2^(N-1) - 1, where N is the ADC's number…
Other Parts Discussed in Thread: ADS5401 Hi,
My cutomer is using ADS5401. He has question about auto correction function. Could you answer me the following questions, please?
Q1: When does auto correction finish? Datasheet shows the sequence of start…
Other Parts Discussed in Thread: ADS5401 Hi,
My customer is consider to use the ADS5401 and has a question.
Input clock amplitude is defined 2Vpp on the datasheet.
Could you show me the voltage range of the input clock?
Best Regards,
Kuramo…
Hi,
I posted same question following thread.
e2e.ti.com/.../545215
If you have any advice from clock side, please let me know.
-------------------------
I received the following question from my customer.
Could you tell me input capacitance…
Other Parts Discussed in Thread: ADS5401 Hi, My cutomer is using ADS5401. He has question about internal LVDS termination.
"8.6.11 Register Name: 3A - Address: 0x3A" in datasheet page of 32 shows about LVDS setting. We would like to know about "Internal…
Hi,
Customer has questions about device Initialization Timing include ENABLE pin operation.
Customer drives ENABLE pin from external. It is low logic at start up.
In datasheet, Figure 2 shows Device Initialization Timing. And, At start up, Sleep…
Other Parts Discussed in Thread: ADS5401 I'd like to inquire about the ADS5401's track and hold operation. I've read the ADS5401 data sheet (SLAS946A - APRIL 2013 - REVISED JANUARY 2014), and, from the diagram on p. 24, I see that the track and hold circuitry…
Other Parts Discussed in Thread: ADS5401 I'd like to verify my understanding of the ADS5401 interleaved ADC pair's operation. I've read through the ADS5401 data sheet (SLAS946A - APRIL 2013 - REVISED JANUARY 2014), and, from the diagram on p. 24, I see…
Hi,
I have asked the design manager for an equivalent input circuit for the clock input of the device. We sometimes have such an equivalent circuit listed in the datasheet but for this device we did not. I suspect that internal loading on the clock…